公告

大中华汽车电子生态圈社区并入开发者社区- 更多资讯点击此

Tip / 登入 to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
zhji_4006061
Level 3
Level 3
25 replies posted 50 sign-ins First solution authored

我们的设备挂了一个i2c的传感器,psoc6当master,通过以下的示例代码来读写传感器的寄存器

{

 
uint8_t readBuffer [5UL];
uint8_t writeBuffer[2UL] = {0U, 5U};
 
/* Configure write transaction */
transfer.slaveAddress = 0x08U;
transfer.buffer = writeBuffer;
transfer.bufferSize = sizeof(writeBuffer);
transfer.xferPending = true; /* Do not generate Stop condition at the end of transaction */
 
/* Initiate write transaction.
* The Start condition is generated to begin this transaction.
*/
(void) Cy_SCB_I2C_MasterWrite(SCB3, &transfer, &i2cContext);
 
/* Wait for transaction completion */
while (0UL != (CY_SCB_I2C_MASTER_BUSY & Cy_SCB_I2C_MasterGetStatus(SCB3, &i2cContext)))
{
}
 
/* Configure read transaction */
transfer.buffer = readBuffer;
transfer.bufferSize = sizeof(readBuffer);
transfer.xferPending = false; /* Generate Stop condition the end of transaction */
 
/* Initiate read transaction.
* The ReStart condition is generated to begin this transaction because
* previous transaction was completed without Stop.
*/
(void) Cy_SCB_I2C_MasterRead(SCB3, &transfer, &i2cContext);
 
/* Wait for transaction completion */
while (0UL != (CY_SCB_I2C_MASTER_BUSY & Cy_SCB_I2C_MasterGetStatus(SCB3, &i2cContext)))
{
}
}
 
但调试中发现有很大概率在下面的代码中死循环,
while (0UL != (CY_SCB_I2C_MASTER_BUSY & Cy_SCB_I2C_MasterGetStatus(SCB3, &i2cContext)))
{
}
请问这是啥原因呢?是i2c初始化没做好?还是i2c总线上有冲突?(但总线上我就挂了一个设备)谢谢!
0 点赞
1 解答
YuZh
Moderator
Moderator
Moderator
100 replies posted 10 likes received 50 sign-ins

Hi:

根据你说的这个现象,会不会跟你连接的GSENSOR有关系,你可以仔细按下他的技术手册,对于初始化是不是需要一个上电的稳定时间之类的。

 

zhichai

在原帖中查看解决方案

6 回复数
zhji_4006061
Level 3
Level 3
25 replies posted 50 sign-ins First solution authored

死循环一般发生在系统刚上电初始化的时候

0 点赞
YuZh
Moderator
Moderator
Moderator
100 replies posted 10 likes received 50 sign-ins

Hi:

1、你是每次上下电都会这样吗?还是只是系统复位才会这样?

2、·用的是什么平台软件,PSOC Creator?还是MTB?我们有对应的example,是否又对照过例程进行调试?

3、有抓过I2C波形吗?建议最好看下。

0 点赞
zhji_4006061
Level 3
Level 3
25 replies posted 50 sign-ins First solution authored

谢谢回复!

1、并不是每次上下电都这样,有80%的概率会死循环

2,我们用的是psoc creator,仿照的例程是CE220818_I2C_Master_High_Level01

3,I2c波形还没抓过,我等下用示波器看下

 

 

0 点赞
YuZh
Moderator
Moderator
Moderator
100 replies posted 10 likes received 50 sign-ins

Hi:

1、你接的是什么I2C设备?

2、你现在测试是注释掉全部其他代码,单独测试I2C吗?

3、你是在自己的硬件板子上测试?

4、抓个波形看看吧,一起分析下。

 

zhichao

0 点赞
zhji_4006061
Level 3
Level 3
25 replies posted 50 sign-ins First solution authored

1, 我们接的是GSENSOR芯片 DA217

2,测试时 其他代码都注释掉了,仅剩一些GPIO和PWM的初始化操作

3,是我们自己的硬件板子

4,波形还在抓

还有我发现在I2C初始化前,延时100ms后就不会死循环了,试了100多次都是正常的,代码如下:

/***************************I2C 配置*****************************/
Cy_SysLib_Delay(100);

I2C_0_Start();

0 点赞
YuZh
Moderator
Moderator
Moderator
100 replies posted 10 likes received 50 sign-ins

Hi:

根据你说的这个现象,会不会跟你连接的GSENSOR有关系,你可以仔细按下他的技术手册,对于初始化是不是需要一个上电的稳定时间之类的。

 

zhichai