Announcements

Ever wondered how you could shape the future in collaboration with others? Join us at OktoberTech Asia Pacific and get inspired. Click here to sign up FREE of charge.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 6 Forum Discussions

JeHa_3912621
Level 3
25 replies posted 10 replies posted 10 questions asked
Level 3

*** Using Compiler 'V5.06 update 6 (build 750)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'

Build Project 'M4' - Target 'Target 1'

linking...

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\cy8c6xx7_cm4_dual.scat(126): warning: L6314W: No section matches pattern *(.cy_app_signature).

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\cy8c6xx7_cm4_dual.scat(136): warning: L6314W: No section matches pattern *(.cy_em_eeprom).

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\cy8c6xx7_cm4_dual.scat(145): warning: L6314W: No section matches pattern *(.cy_sflash_user_data).

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\cy8c6xx7_cm4_dual.scat(154): warning: L6314W: No section matches pattern *(.cy_sflash_nar).

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\cy8c6xx7_cm4_dual.scat(163): warning: L6314W: No section matches pattern *(.cy_sflash_public_key).

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\cy8c6xx7_cm4_dual.scat(172): warning: L6314W: No section matches pattern *(.cy_toc_part2).

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\cy8c6xx7_cm4_dual.scat(181): warning: L6314W: No section matches pattern *(.cy_rtoc_part2).

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\cy8c6xx7_cm4_dual.scat(191): warning: L6314W: No section matches pattern *(.cy_xip).

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\cy8c6xx7_cm4_dual.scat(201): warning: L6314W: No section matches pattern *(.cy_efuse).

Program Size: Code=13182 RO-data=2174 RW-data=692 ZI-data=109224 

Finished: 0 information, 9 warning and 0 error messages.

FromELF: creating hex file...

After Build - User command #1: C:\Keil_v5\ARM\PACK\Cypress\Pack\2.0.0\Device\CY8C6347BZI-BLD53_Pack\Other\postbuildCortexM4.bat "E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\ObjectsM4\M4.axf" "E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\ObjectsM4\" "E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\" "cmsis" "C:\Keil_v5\ARM\PACK\Cypress\Pack\2.0.0\Device\CY8C6347BZI-BLD53_Pack\Other\win\elf"

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild>IF /I "cmsis" NEQ "cmsis" GOTO not_cmsis

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild>copy /Y "C:\Keil_v5\ARM\PACK\Cypress\Pack\2.0.0\Device\CY8C6347BZI-BLD53_Pack\Other\win\elf\cymcuelftool.exe" "E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\\cymcuelftool.exe"

已复制         1 个文件。

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild>move /Y "E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\ObjectsM4\M4.axf" "E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\ObjectsM4\\M4_link.axf"

移动了         1 个文件。

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild>for %i in ("E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\\Objects\*_link.axf") do @(IF "%i" NEQ "E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\ObjectsM4\\M4_link.axf" set MergeFiles=!MergeFiles! "%i" )

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild>set MergeFiles="E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\ObjectsM4\\M4_signed.axf"

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild>"E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\\cymcuelftool.exe" --sign "E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\ObjectsM4\\M4_link.axf" --output "E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\ObjectsM4\\M4_signed.axf"

No ELF section .cychecksum found, creating one

Application checksum calculated and stored in ELF section .cychecksum

Checksum calculated and stored in ELF section .cymeta

E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild>"E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\\cymcuelftool.exe" --merge "E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\ObjectsM4\\M4_signed.axf" --output "E:\Work\18.reflex-PPG\Software\Cypress-Prj\Cy-V0.001\VitaBle.cydsn\uVisionBuild\ObjectsM4\M4.axf"

Expected at least 2 elf file arguments for -M/--merge

Usage:

Display help:

   cymcuelftool -h/--help

Display version information:

   cymcuelftool -v/--version

Display memory allocation by type:

   cymcuelftool -A/--allocation file.elf

Merge ELF files:

   cymcuelftool -M/--merge complete_app1.elf complete_app2.elf ... [--output merged.elf] [--hex merged.hex]

Sign ELF file, with option for secure (encrypted) signature:

   cymcuelftool -S/--sign unsigned.elf [<SignScheme>] [--output signed.elf] [--hex signed.hex]

Generate Patch file:

   cymcuelftool -P/--patch file.elf [--encrypt <Cipher*> --key key.txt [--iv iv.txt]] [--output patch.cyacd2]

   *NOTE: RSAES-PKCS and RSASSA-PKCS not allowed for this command

Create Code sharing file:

   cymcuelftool -R/--codeshare file.elf symbols.txt <GCC/ARMCC/IAR> [--output shared.s]

<SignScheme> is only used for signing the user application. It must be ONE of:

   1) HMAC <Hash*>  --key key.txt              (*CRC not supported)

   2) CMAC-AES-XXX* --key key.txt              (*XXX can be 128, 192, or 256)

   3) <Hash> [--encrypt <Cipher> --key key.txt [--iv iv.txt]]

<Hash>: CRC, SHA1, SHA224, SHA256, SHA384, SHA512

<Cipher> (requires key):

   Public-key: RSAES-PKCS, RSASSA-PKCS

   Symmetric:  DES-ECB, TDES-ECB, AES-{128|192|256}-{ECB|CBC|CFB}

key.txt: ASCII text file containing key appropriate for chosen Cipher. May be symmetric hex key or PEM format for RSA cipher variants

iv.txt:  ASCII text file containing initialization vector for certain encryption algorithms

".\ObjectsM4\M4.axf" - 0 Error(s), 9 Warning(s).

Build Time Elapsed:  00:00:02

0 Likes
1 Solution
RyanZhao
Moderator
Moderator 100 sign-ins 100 likes received First comment on KBA
Moderator

I think you're using µVision 5, when you exporting, select  CMSIS-Pack Projects

View solution in original post

0 Likes
2 Replies
RyanZhao
Moderator
Moderator 100 sign-ins 100 likes received First comment on KBA
Moderator

Hi Jerry, Could you double-check your project exporting with using PSoC Creator?

PSoC Creator's help file provided good guidance on this exporting. Please do not ignore any steps described in the help menu.

0 Likes
RyanZhao
Moderator
Moderator 100 sign-ins 100 likes received First comment on KBA
Moderator

I think you're using µVision 5, when you exporting, select  CMSIS-Pack Projects

0 Likes