Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 6

John_K
Level 3
First like received 25 sign-ins 10 replies posted
Level 3

Is it possible to disable IMO in PSOC6 (assuming that clock HF clocked is switched to ECO like ALTHF)?

I didn't see any API (in PDL) that allows shutting it down.

  I think it was possible in PSOC4, and we did this for lower power (when running off ECO).

 

 

 

0 Likes
1 Solution
Ekta
Moderator
Moderator 250 sign-ins First question asked 500 replies posted
Moderator

Hello @John_K ,

In case of PSoC 6 the IMO will be automatically disabled when moving the device to low power mode (Deep Sleep and Hibernate) as can be seen in the image attached:

Ekta_0-1626443299485.png

It is possible to disable IMO by setting the Enable bit of the CLK_IMO_CONFIG register to low but it is not recommended to do so. This bit must be high at all times for all functions to work properly. Hardware will automatically disable the IMO during HIBERNATE and XRES. It will automatically disable during DEEPSLEEP if DPSLP_ENABLE==0.

Thanks 

Ekta

 

 

 

View solution in original post

0 Likes
4 Replies
Top labels