Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

Sort by:
ESCLuisFlores
PSoC™ 6
Hi Infineon community, I'm currently developing a project in ModusToolbox using the CY8CPROTO-063-BLE, along with the Bluetooth_LE_Hello_Sensor. My ai... Show More
ESCLuisFlores
PSoC™ 6
Hi Infineon Community,  I'm experiencing a connection issue with the CY8PROTO-063-BLE when using the AIROC Bluetooth Connect App. On one smartphone, I... Show More
schuetziken
PSoC™ 6
Hello, I work with ModusToolbox via VSCode. I have successfully tested my programme on the CYPROTO-063-BLE kit. To do this, I had to adapt the flash m... Show More
Oliver_Song
PSoC™ 6
Hi all, I had a question while studying the UART function of MTB. I understand that the UART API is divided into two categories: High-level and Low-le... Show More
applepie
PSoC™ 6
I see the latest version of PDL (3.17) for PSOC creator has USB driver and Middleware are from version 1.0. But from PDL API reference I see the curre... Show More
Translation_Bot
PSoC™ 6
I use CY8C6347BZI_BLD53. I use SPI_DMA to transfer data. When I set the SPI speed to less than 15MHz, the transmission is normal. When the SPI speed i... Show More
yossefhaycohen
PSoC™ 6
Hi, We are using a CYB06445LQI-S3D42 device. Starting with a default clock configuration worked well. When we have tried to configure the system clock... Show More
Purush
PSoC™ 6
Hi all, good day. I want to know how to use SEGGER AppWizard GUI Builder Software with CY8CKIT-062-WIFI-BT  in ModusToolbox? I built the GUI and Expor... Show More
djozwiak
PSoC™ 6
I have a custom board that has the CY8C6136BZI-F14 and a TI CC3135 WiFi chip. I have created a custom BSP for the board. Per the information in the BS... Show More
yiru_1705901
PSoC™ 6

我的需求是 是类I2C通信,四个数据线公用一个时钟线,不是QSPI,四个数据线独立发送数据的,时钟大于等于20MHZ,用UDB可以实现吗? 

我使用的芯片是CY8C6247AZI-D54,有12个UDB, 我用IO口模拟的通信如附件。

Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.