PSoC™ 6 Forum Discussions
Hello,
I am using a PSoC 63 BLE Module (CYBLE-416045-02) and I am trying to program it using JTAG by using a MINIPROG4. But I am not sure how I should connect the hardware? To which pins ? Can anyone help please?
Kind regards
Show Less
I would like to fabricate a data logger with CYPROTO-063-BLE.
However, I am a complete beginner.
I would like my data logger to have the following features
・At 100Hz intervals, get sensor data with i2c using DMA
・Save data to SD card
・Send data to cell phone via BLE(Should we separate CM0 and CM4 functions?)
using modustoolbox
Would you be able to give me some examples, tutorials, etc. that would be helpful to me?
Show LessI'm using a miniprog3 with a CY8C6117BZI-F34. Before today, programming and debugging have worked fine. However, today I start "debug" in PSoC Creator 4.4 while power was turned off to the PSoC6 device but the miniprog3 was connected. I then turned on power to the PSoC6 device. Ever since then, Cypress software cannot detect the PSoC6 device. I've tested the miniprog3 on another PCB and it detects PSoC device on that device fine. I've also confirmed that the power supply (3.3V) is good. I've attached a screen capture of what I seen in PSoC Programmer 3.29.1.
Can you help explain this problem? Is there other debug or status that I can do with the Cypress software? Is it possible that power cycling at that time corrupted something in the PSoC6 device? If so, is there any way to recover the device?
Show LessHello,
I am trying to display the value of reflectometer in UART in a separate function other than the main but its not giving any reading. Can you please check the project for me?
Thank you
Show LessHello,
I am using a PSoC 63 BLE Module (CYBLE-416045-02). I will use it in a project and I would like to know how I can interface the kitprog. Can anyone help please?
Thanks
Show LessHello,
Do you have ModusToolbox code example for the PSoC64 BLE Direct Test Mode over HCI?
I have a new project with CYB06447BZI-BLD53 and I will have to test the BLE Radio. We also have plans to do BLE qualification later.
Could I use the CyBluetool 1.0 for testing?
Best Regards,
Gintaras
Show LessHello,
I would like to use an OLED screen in psoc 6 and would like to check if it's possible to use the pins P9[5] and P9[6] to connect it?
Thank you
Show LessThank you
Hi there,
After downloading Cryptography_AES_Demostration example codes from Github, I have tried all AES ECB mode, CBC mode, and CFB mode, all of them works fine.
However, I got some trouble in calling Cy_Crypto_Core_Aes_Ctr. Specifically speaking, I have no idea how to provide the parameters of this API function.
Do you have any example codes to show me how to encrypt/decrypt by AES CTR mode?
Hardware : CY8KIT-062-BLE
ModusToolbox version: 2.4.0
Thanks,
Show Less