PSoC™ 6 Forum Discussions
Hello team,
Hope you are doing well.
- Wanted to confirm that PSoC 62 capable of Secure Boot -> Yes / No
- The datasheet displays standard orderable part numbers. How can we differentiate between standard and 'secure' parts? Table 57 in the datasheet shows CY8Cxxx variants, which are standard parts capable of 'Secure Boot'.
- Would the part numbers change once a device is programmed for secure boot?
Thank you.
Randhir
Show LessHi all,
I'm testing a custom board for the first time and I'm adding components as I test . I have a crystal and caps for the ECO and this works. A couple of LEDs connected to P8.2 and P8.3 blink according to my code. I also have a crystal and caps for the WCO but I haven't tested the WCO. I added an external oscillator (ExtOsc) to pin P0.5 and I discover that its trace is too close to the WCO crystal. If the WCO is enabled nothing works. So while testing I disabled the WCO and the ExtOsc almost worked. I started by setting all the MUXs (in the system tab in device configurator, modustoolbox latest version) to ExtOsc but I got this error after programming: DP initialization failed. After a few minutes of testing I found that I get this error if I set MUX_PATH2 to ExtOsc. If I set all MUXs to ExtOsc (except MUX_PATH2. MUX_PATH2 set to ECO) I don't get the error and the LEDs blink. MUX_PATH2 goes to one of the PLLs and there are more settings there that I haven't changed. Is this a setting problem in the PLL connected to MUX_PATH2? I don't even know what the error means. How do I fix this?
Thanks
Show LessHello everyone:
I have a very urgent and difficult question.
I use the Modus Tool2.2 ,but no simulation.
I would like to know if simulation is possible using MODUS Tool.
thank you very much
Show LessHello,
I am configuring the GATT settings in the PSoC creator (BLE component).
I set the "Artibute MTU size (bytes)" to be 512. At the same time, I made a custom service that is containing 7 custom characteristics, as shown in the following figure.
My question is: is it Ok to set the field length of each characteristic to be 500? Because the Attribute MTU size is set to be 512. Seven characteristics with 500 bytes each will be 3500 bytes in total, which is larger than the Attribute MTU size.
When I set it as 500, and build the project, the PSoC Creator shows the project is successfully built. However, the BLE stack seems stuck during running (sending notifications).
Thank you very much for your kindly help!
Show LessIam trying to find compiler optimization in modustoolbox, not yet found.
I found that on editing CFLAGS variable in the make file will works, but still iam unable to see the optimized code.
Can you please guide me on this ?
Thanks inadvance.
Show LessHello everyone,
I'm working on a project with CYCLE-416045-02 and i'm using bluetooth.
I used the xTimer available in the defaut file for CYCLE-416045-02 BLE to generate a led blink when my uC advertising.
I want to use 2 new leds and i want that they blink.
So for that i have created 2 new Timer and configure my status_led_task.
My problem is the following, when my uC advertising all work good. When advertising finnish all led stop blink but i expected that only advertising led stop to blink.
After different try and modification in my code and don't have find any solution.
Could you tell me if you have advice or if you have meet this problem ?
Best regards,
Max
Show Less
Hi.
I'm using CY8C6137BZI-F54 at my design.
I have 15 analog inputs that are connected to port 9,10.
When I put the pin assignment all the analogs at port 9, there is a worning about routing congestion.
What do I need to do?
BR
Shmuel
Show LessHello,
I have the CY8CEVAL-062S2 with LAIRD M.2 module and running MTB 2.4. If I create any Bluetooth example with the PSoC6 BSP = CY8CEVAL-062S2-LAI-4373M2, I'm unable to open the Bluetooth Configurator in that example. The error message is:
Unable to run external editor: Unable to launch configurator: ../mtb_shared/core-make/release-v1.9.1/make/core/open.mk:179: *** Unsupported tool type - bt-configurator.
Supported types are: capsense-configurator capsense-tuner device-configurator dfuh-tool library-manager ml-configurator project-creator qspi-configurator seglcd-configurator smartio-configurator usbdev-configurator. Stop.
The same error happens if BSP = CY8CEVAL-062S2-MUR-43439M2.
But if BSP = CY8CKIT-062S2-43012, then the Bluetooth Configurator 2.50 can be launched successfully.
What could be wrong?
Thanks!
Show LessWe are evaluating ADC using CY8CKIT-062S2-43012. How can we evaluate multi input ADC feature on PSoC6?
We are evaluating ADC using CY8CKIT-062S2-43012. Please tell me the ADC input signal voltage range.