Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

riccardo-monty
PSoC™ 6
Hi, I'd like to know is it right? When I change bsp mcu target, from default CY8C6244LQI-S4D92 to CY8C6244AZI-S4D93, I can program the kit successfull... Show More
wwpl
PSoC™ 6
Hi,  Understand that this example project "PSoC 6 MCU with BLE Connectivity: Battery Level (FreeRTOS)" works with PSoC 6 BLE Prototyping Kit (CY8CPROT... Show More
scollyer
PSoC™ 6
I have a project that's using an external sync clock signal that I want to use an input to a counter. The signal of interest is connected to the P7.6 ... Show More
vim_2255711
PSoC™ 6
Hi,  Framework MTB SDKBoard:PSoc 62S2I tried connect to hidden ssid  by giving only mac address, security type and channel number and SSID len as with... Show More
deepakhm09
PSoC™ 6
Hi, In we are using PSoC 6 Controller in one of our project, So I tried installing Modus Toolbox in my linux machine as suggested in the user guide. A... Show More
CoreyW_81
PSoC™ 6
In PDL CAT1 version 2.4.1, there is a define, CY_DELAY_MS_OVERFLOW, that is defined in cy_syslib.h. However, in PDL version 3.0.0, that define has no... Show More
matthiasb
PSoC™ 6
Hello, i'm trying to minimize the power usage of our Psoc6 based ble-enabled battery-powered pcb. I made use of the ULP mode and lower CPU Frequency a... Show More
vivekatamantya
PSoC™ 6
Hello community members,I have been using ModusToolBox 2.4 for the last 6 months, but still trying to solve why indexing is not working in ModusToolBo... Show More
Rodo
PSoC™ 6
Hi all, MTB3.0 is ModusToolBox 3.0 I have a custom board that works with MTB2.4 (and MTB3.0). Now I'm using MTB3.0 and I'm programming the board. The ... Show More
conradc2380
PSoC™ 6
Hi ,   I have been spending the last few days trying to figure out  how to increase the flash size according to the linkers scripts for GCC -Arm compi... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.