Dears,
I would like to test FPU in PSOC6 in modus toolbox 2.4 environment
I installed CMSIS DSP and set all variables in makefile (DEFINES, INCLUDES, LDLIBS as noted in another posts like https://community.infineon.com/t5/PSoC-6/How-to-use-ARM-CMSIS-DSP-lib-in-ModusToolbox2-4/m-p/342494 ...) when VFP_SELECT=hardfp all source codes compiles ok and project seems to run normally but I still think that FPU is not used... So I would like also test with "software emulated" and compare execution time.
But when I set makefile variable VFP_SELECT=softfp or to empty value (as default) But now I got compilation errors like this "ld.exe: failed to merge target specific data of file...":
Linking output file mtb-example-psoc6-lptimer.elf
c:/users/xxx/modustoolbox/tools_2.4/gcc/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: error: ../CMSIS/DSP//Lib/GCC/libarm_cortexM4lf_math.a(arm_sin_f32.o) uses VFP register arguments, C:/Users/xxxx/mtw/Low-Power_Timer/build/CY8CKIT-062-WIFI-BT/Debug/mtb-example-psoc6-lptimer.elf does not
c:/users/xxx/modustoolbox/tools_2.4/gcc/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: failed to merge target specific data of file ../CMSIS/DSP//Lib/GCC/libarm_cortexM4lf_math.a(arm_sin_f32.o)
c:/users/xxx/modustoolbox/tools_2.4/gcc/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: error: ../CMSIS/DSP//Lib/GCC/libarm_cortexM4lf_math.a(arm_cos_f32.o) uses VFP register arguments, C:/Users/xxx/mtw/Low-Power_Timer/build/CY8CKIT-062-WIFI-BT/Debug/mtb-example-psoc6-lptimer.elf does not
c:/users/xxx/modustoolbox/tools_2.4/gcc/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: failed to merge target specific data of file ../CMSIS/DSP//Lib/GCC/libarm_cortexM4lf_math.a(arm_cos_f32.o)
c:/users/xxx/modustoolbox/tools_2.4/gcc/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: error: ../CMSIS/DSP//Lib/GCC/libarm_cortexM4lf_math.a(arm_mult_f32.o) uses VFP register arguments, C:/Users/xxx/mtw/Low-Power_Timer/build/CY8CKIT-062-WIFI-BT/Debug/mtb-example-psoc6-lptimer.elf does not
c:/users/xxx/modustoolbox/tools_2.4/gcc/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: failed to merge target specific data of file ../CMSIS/DSP//Lib/GCC/libarm_cortexM4lf_math.a(arm_mult_f32.o)
c:/users/xxx/modustoolbox/tools_2.4/gcc/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: error: ../CMSIS/DSP//Lib/GCC/libarm_cortexM4lf_math.a(arm_add_f32.o) uses VFP register arguments, C:/Users/xxx/mtw/Low-Power_Timer/build/CY8CKIT-062-WIFI-BT/Debug/mtb-example-psoc6-lptimer.elf does not
c:/users/xxx/modustoolbox/tools_2.4/gcc/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: failed to merge target specific data of file ../CMSIS/DSP//Lib/GCC/libarm_cortexM4lf_math.a(arm_add_f32.o)
c:/users/xxx/modustoolbox/tools_2.4/gcc/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: error: ../CMSIS/DSP//Lib/GCC/libarm_cortexM4lf_math.a(arm_common_tables.o) uses VFP register arguments, C:/Users/xxx/mtw/Low-Power_Timer/build/CY8CKIT-062-WIFI-BT/Debug/mtb-example-psoc6-lptimer.elf does not
c:/users/xxx/modustoolbox/tools_2.4/gcc/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: failed to merge target specific data of file ../CMSIS/DSP//Lib/GCC/libarm_cortexM4lf_math.a(arm_common_tables.o)
collect2.exe: error: ld returned 1 exit status
make[1]: *** [../mtb_shared/core-make/release-v1.9.1/make/core/build.mk:529: C:/Users/xxx/mtw/Low-Power_Timer/build/CY8CKIT-062-WIFI-BT/Debug/mtb-example-psoc6-lptimer.elf] Error 1
make: *** [../mtb_shared/core-make/release-v1.9.1/make/core/main.mk:434: secondstage_build] Error 2
"C:/Users/xxx/ModusToolbox/tools_2.4/modus-shell/bin/make CY_MAKE_IDE=eclipse CY_MAKE_IDE_VERSION=2.4 CY_IDE_TOOLS_DIR=C:/Users/xxx/ModusToolbox/tools_2.4 -j12 all" terminated with exit code 2. Build might be incomplete.
What is going bed ?
Best Regards
Radim
Show Less
Hi
I made custom BSP for CY8C6244AZI-S4D93.
I was trying to add DAC configuration using MTB but I think there are some problem with connection verification.
According to below diagram, direct output of DAC is able to connect with pin 6 of CTB port.
In this IC, CTB port is port 9 and pin 6 is not available.
so the other way to make output path of DAC is using buffer.
as you can see in following picture. When I set DAC output as buffered output, there is only one option that I could choose to use as DAC output path is v plus of opamp0.
but the indicator always shows me yellow light even I tried every other combination of connections.
of course I tried it after disabled all other peripherals even the debugging port.
could you check this point?
Show LessHi All,
In the case of the CYB06445LQI-S3D42 product, is there any data that shows how many ms it takes to 'Secure Boot'
from the device reset to the user application starts?
Even rough information is fine.
Best regards,
Alex Park.
Show Less
I would like to confirm my observation when calling the Cy_Crypto_Core_ECC_SignHash() and Cy_Crypto_Core_ECC_MakeKeyPair() functions. The Cy_Crypto_Core_ECC_MakeKeyPair() returns the public key (X & Y) in little endian format, same for the signature (R & S) returned by the Cy_Crypto_Core_ECC_SignHash() function. I verified this by using Mbedtls to generate the public key from a private key created by Cy_Crypto_Core_ECC_MakeKeyPair().
Show Less
Hi.
I'm trying to use the HAL System Power Management library to put the CM4 to sleep. So far, I've had no luck, and as I have found too many times, there is very little documentation available, and no examples. What documentation exists (e.g. Architecture TRM) is unclear, even suggesting that only masked interrupts can wake up a sleeping CPU.
Here's the environment:
The first problem is that the CPU either doesn't sleep, or wakes up immediately. I disable the RTOS SysTick interrupt in one of the callbacks. I also disable several other peripheral interrupts, and turn off the BLE stack, none of which has made a difference. It's likely that some interrupt is firing, but I can't think of a good way to determine which is the culprit.
The second problem is that the stated behavior, namely that the callbacks are called on wakeup (CYHAL_SYSPM_AFTER_TRANSITION) in the reverse of the order in which they are called on sleep (CYHAL_SYSPM_CB_CPU_SLEEP) does not match the observed behavior.
Callbacks are always called in the same order, even when one of the callbacks returns false in response to CYHAL_SYSPM_CHECK_READY.
Has anyone successfully used cyhal_syspm_sleep() to put one of the CPUs to sleep?
Thanks,
-Nick
Show LessI'm using a a CY8CKIT-062-BLE with the EINK display.
I have two projects using this kit.
One works to update the display the other does not.
On the one that doesn't work (link) it complains about a code line using:
LCD_GetDisplayBuffer().
The linker complains and aborts:
.\CortexM4\ARM_GCC_541\Debug\main_cm4.o: In function `UpdateDisplay':
C:\Users\lpoma\Desktop\SineGen_Audio\SineGen_Audio_EINK_062-BLE.cydsn/main_cm4.c:174: undefined reference to `LCD_GetDisplayBuffer'
collect2.exe: error: ld returned 1 exit status
The command 'arm-none-eabi-gcc.exe' failed with exit code '1'.
I compared the build specs of the two projects and the issue is not immediately apparent.
Apparently I'm missing a em-Win library reference some where.
I can use some expert help here.
Thanks in advance.
Show LessPSoC 6 MCU: CY8C62x6,
CY8C62x7 Datasheet
I think that it was printed incorrectly in Address Map. Page 12 of 77
0xE010 0A000 – 0xFFFF FFFF Device Device-specific system
registers.
PSoC 6 MCU: CY8C62x6, CY8C62x7 Datasheet (infineon.com)
Show LessHello,
I have questions about Flash and Emulated EEPROM.
1. The flash endurance is described in the datasheet as 100k cycles.
Does each row of flash individually have 100k cycle endurance?
2. I'm using the Emulate_EEPROM example in modus toolbox. (CY8CKIT-062-WIFI-BT)
Please let me know how it works internally when using Em_EEPROM.
I want to know about the case of repeatedly writing a few bytes of data to the same address.
For example, when only a few bytes are to be written, will the entire line (512 bytes) including this address be erased and re-written?
Does the Em_EEPROM algorithm read the entire existing row of data into RAM before it is deleted, then modify only a few bytes and write it to flash?
Thanks and Regards,
YS
Dear Receiver,
I practice "PSoC™ 6 MCU: MCUboot-based basic bootloader" by using the example code in the following GitHub link...
https://github.com/Infineon/mtb-example-psoc6-mcuboot-basic
I follow the steps and I can run boot, app (boot mode), and app (upgrade mode), separately.
But I feel confused about...
when I reset the board, there are no any response in the UART communication. Besides, LED blinking is also no response.
I think every time I reset MCU, it should enter boot mode. If no new image be found, it will enter app mode automatically.
in my test, it seems no any other response if I reset the board. I am sure boot code is in the CM0+ and app code is in the
CM4. Once I reset the board, boot code and app code seem disappear.
Could you please explain this phenomenon for me ?!
Thank you so much.
Show Less
Dear Expert.
Hello. I have a question as below.
I'm trying to use the emwin Driver provided in PSOC6. (pre included Driver at MTB IDE)
1. Is there a extra cost to implement the graphic function using the driver? Or is it available for free?
Please help.
Show LessUser | Count |
---|---|
64 | |
46 | |
13 | |
12 | |
11 |