Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

Rodo
PSoC™ 6
Hi all, MTB3.0 is ModusToolBox 3.0 I have a custom board that works with MTB2.4 (and MTB3.0). Now I'm using MTB3.0 and I'm programming the board. The ... Show More
conradc2380
PSoC™ 6
Hi ,   I have been spending the last few days trying to figure out  how to increase the flash size according to the linkers scripts for GCC -Arm compi... Show More
suryasundar96
PSoC™ 6
Hi I am using CY8CPROTO-062-4343W board I downloaded Wi-Fi scan program in ModusToolbox ide .While tracing the code in UART it showing like below. How... Show More
jsmith678x
PSoC™ 6
Hi, I'm trying to debug code on CY8CPROTO-063-BLE board but it doesn't work. Is it possible to hw debug on CY8CPROTO-063-BLE? I tried with ModusToolbo... Show More
qp
PSoC™ 6
Dear Community. Please give me some advice on my problem. When I try to create a new project file using the project creator, I get the following e... Show More
Nirmith
PSoC™ 6
Hi, I have attached an attachment which consists of the pin mapping of PSoC 6. As I have mapped but I don't know if its correct or not can you help me... Show More
gryfin_chen
PSoC™ 6
I use CY8CKIT-064B0S2-4343W to run some examples in this project "Secure_Blinky_LED_FreeRTOS" When I execute following command (Secure Boot), I get an... Show More
pblemel
PSoC™ 6
Hello, everyone! Although this is more of a PDL question than a PSoC question, I'm moving this question here, since I'm working with the PSoC 6.  Usin... Show More
Frank_vec
PSoC™ 6
1  psoc62+connectivity 是目前流行的 wifi BLE方案 如上图所示,是可以的,并且是官方推荐的  2  如果是PSOC63芯片,则默认的 connectivity 是无连接的 ,现在客户有个想法 是 PSOC63芯片+CYW43012,二者通过SDIO 接口来连接,请问硬... Show More
Rodo
PSoC™ 6
My project is set up with local git. It is self contained so it does not use the share folder. It works... actually it builds without errors. I still ... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.