Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

vivekatamantya
PSoC™ 6
Hello Infineon Community,I have been working with PSoC 6-based CY8C6244LQQ-S4D92 microcontroller. The issue with this MCU is happening when I am tryin... Show More
KC1SA
PSoC™ 6
a few years back I did this, but I've lost track of where I got the utility.  I need to put an image on the display.  From my recollection I had to ta... Show More
Manoj_Kumar
PSoC™ 6
I wish to upload the written code into my Psoc6 through UART and it should load into bootloader and load the program . How can i do so?   Show More
conradc2380
PSoC™ 6
Hi , I am working on the PSOC62 free-running WDT , I followed the example in the following link to use the PDL as i am working on the CM0. https://github.com/Infineon/Code-Examples-for-the-ModusToolbox-PSoC-6-SDK/blob/mt1.1/CE220060_PSoC6_WatchdogTimer/Source/main.c... Show More
paulbart1234
PSoC™ 6
Hello -I’ve been using the CY8C6247BZI-D54 in a project for a while.  My code loads/runs/I can debug it (using PSoC Creator) just fine.We just got new... Show More
magnus
PSoC™ 6
Hi, I am trying to integrate a bootloader into my project and started with the "MCUboot-Based Basic Bootloader". However, I encountered an issue durin... Show More
Manoj_Kumar
PSoC™ 6
I am trying to create the bootloader build in example, but its giving me this error. ERROR:Failed to export the "MCUboot_based_Basic_Bootloader_for_PS... Show More
shepdog87
PSoC™ 6
I am using the MODUS IDE because my PSOC 62 kit / is not available in PSOC Creator. I am trying to chain 2 DMA components together using the HAL drive... Show More
VarunK_66
PSoC™ 6
Hi Team,  I'm working on a use case where I have to run MQTT, HTTPs applications on the CM0p core of my PSoC 6 (2M part). I see that the code examples... Show More
azBlock1
PSoC™ 6
I am using v3.0 tools and visual studio code. This is more of a bug report but also a reference for anyone hitting this problem themselves. I have a c... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.