Hi,
I am developing a low-power application using CY8CKIT-062-BLE board.
I followed the application note "PSoC 6 MCU Device Firmware Update Software Development Kit Guide" and configured a "map A" BLE DFU Memory Maps.
On the basis of above configuration, I am trying to use the non-volatile memory of PSoC by following the example code : CE220120
So, In the App1, I declare a const value before the "main()" function:
CY_ALIGN(CY_FLASH_SIZEOF_ROW)
const uint8_t flashData[CY_FLASH_SIZEOF_ROW] = {0}; /* The array will be placed in Flash */
Then in the the "main()" function, I write the following code:
uint8_t ramData[CY_FLASH_SIZEOF_ROW];
Initial_finished=false;
/* Initialize the data in RAM that will be written into flash */
for(uint16_t index = 0; index < CY_FLASH_SIZEOF_ROW; index++)
{
ramData[index] = (uint8_t)index;
}
cy_en_flashdrv_status_t flashWriteStatus;
flashWriteStatus = Cy_Flash_WriteRow((uint32_t)(flashData), (const uint32_t *)ramData);
The App1 properly works after updating the App0 to App1.
However, after I powered off the board and powered on again (or put RESET button ), the system cannot execute App1 properly; it keeps in App0 and waiting for updating image.
I called printf to check what is wrong, and found after resetting, in App0 "status = Cy_DFU_ValidateApp(1u, &dfuParams)", the status is not "CY_DFU_SUCCESS".
If I remove the "Cy_Flash_WriteRow()" function in App1, the App1 can be normally executed after resetting the system.
So my question is:
1. What makes "Cy_DFU_ValidateApp(1u, &dfuParams)" failed after calling "Cy_Flash_WriteRow()" in App1?
2. How to make sure "Cy_DFU_ValidateApp(1u, &dfuParams)" not failed after calling "Cy_Flash_WriteRow()" in App1?
Thank you very much for your kind help!!
Best regards,
Jiabin
Show LessI'm just trying to get some I2C comms going on a CY8C6247FDI-D32 as SCB0. SCL is on P0[2] and SDA is on P0[3]. Ive tried setting the pin mux for them to be GPIO and I can see the pins toggling so our wiring is OK.
Running the code, SCL is high and stays that way. And I get timeout errors on the I2C calls. I dont see where I'm doing anything other than the examples I stole the code from.
What am I missing?
static cy_stc_scb_i2c_context_t i2cContext;
const cy_stc_scb_i2c_config_t i2cConfig =
{
.i2cMode = CY_SCB_I2C_MASTER,
.useRxFifo = false,
.useTxFifo = false,
.slaveAddress = 0U,
.slaveAddressMask = 0U,
.acceptAddrInFifo = false,
.ackGeneralAddr = false,
.enableWakeFromSleep = false,
.enableDigitalFilter = false,
.lowPhaseDutyCycle = 8U,
.highPhaseDutyCycle = 8U,
};
Cy_SCB_I2C_Init(SCB0, &i2cConfig, &i2cContext);
/* Connect SCB0 I2C function to pins */
Cy_GPIO_SetHSIOM(I2C_SCL_PORT, I2C_SCL_NUM, P0_2_SCB0_I2C_SCL);
Cy_GPIO_SetHSIOM(I2C_SDA_PORT, I2C_SDA_NUM, P0_3_SCB0_I2C_SDA);
/* Configure pins for I2C operation */
Cy_GPIO_SetDrivemode(I2C_SCL_PORT, I2C_SCL_NUM, CY_GPIO_DM_OD_DRIVESLOW);
Cy_GPIO_SetDrivemode(I2C_SDA_PORT, I2C_SDA_NUM, CY_GPIO_DM_OD_DRIVESLOW);
Cy_SysClk_PeriphAssignDivider(PCLK_SCB0_CLOCK, CY_SYSCLK_DIV_8_BIT, 1);
Cy_SysClk_PeriphSetDivider(CY_SYSCLK_DIV_8_BIT, 1, 31);
Cy_SysClk_PeriphEnableDivider(CY_SYSCLK_DIV_8_BIT, 1);
uint32_t inputClockFrequency = Cy_SysClk_PeriphGetFrequency(CY_SYSCLK_DIV_8_BIT, 1);
uint32_t currentDataRate = Cy_SCB_I2C_SetDataRate(SCB0, 100000, inputClockFrequency);
if ((currentDataRate > 100000) || (currentDataRate == 0)) {
CY_ASSERT(0);
}
Cy_SCB_I2C_Enable(SCB0);
Cy_SCB_I2C_MasterSendStart(SCB0, 0x48, CY_SCB_I2C_WRITE_XFER, 1000, &i2cContext);
Cy_SCB_I2C_MasterWriteByte(SCB0, 0xAA, 1000, &i2cContext);
Cy_SCB_I2C_MasterSendStop(SCB0, 1000, &i2cContext);
Hi,
We are trying to port the existing firmware in PSOC Creator to ModusToolbox to make it available for the new chips.
However, the biggest challenge we are facing right now is the Analog Multiplexer that's not available in ModusToolbox as it is in PSOC Creator.
I'm wondering if there is any example on how to use the AMUX in ModusToolbox?
Any help will be much appreciated.
Thanks in advance.
GP
Show LessI would like to confirm my observation when calling the Cy_Crypto_Core_ECC_SignHash() and Cy_Crypto_Core_ECC_MakeKeyPair() functions. The Cy_Crypto_Core_ECC_MakeKeyPair() returns the public key (X & Y) in little endian format, same for the signature (R & S) returned by the Cy_Crypto_Core_ECC_SignHash() function. I verified this by using Mbedtls to generate the public key from a private key created by Cy_Crypto_Core_ECC_MakeKeyPair().
Show Less
Hello,
I have questions about Flash and Emulated EEPROM.
1. The flash endurance is described in the datasheet as 100k cycles.
Does each row of flash individually have 100k cycle endurance?
2. I'm using the Emulate_EEPROM example in modus toolbox. (CY8CKIT-062-WIFI-BT)
Please let me know how it works internally when using Em_EEPROM.
I want to know about the case of repeatedly writing a few bytes of data to the same address.
For example, when only a few bytes are to be written, will the entire line (512 bytes) including this address be erased and re-written?
Does the Em_EEPROM algorithm read the entire existing row of data into RAM before it is deleted, then modify only a few bytes and write it to flash?
Thanks and Regards,
YS
I use PSOC Creator 4.4 and in the display section I did not find the normal LCD, I have found Graphical only.
Show Lessi debug the program, the program enters the Cy_Syslib_ProcessingFault function.
when the program runs to the
, The program will sure enter cy_ Syslib_ Processingfault function.
When I use a certain value instead of uitemp0, the program will not enter the fault function.
what's the reason? Thanks!
Show LessHi,
I am learning the BLE bonding and pairing by studying the code example "CE212742".
In the StackEventHandle in the example code, there is the following code:
/* Generate new private address automatically */
Cy_BLE_SetResolvablePvtAddressTimeOut(CY_BLE_PVT_ADDRESS_TIMEOUT);
My question is:
1. Will the BLE API automatically renew the private address after this "CY_BLE_PVT_ADDRESS_TIMEOUT"?
2. Will the StackEventHandle receive an event after this "CY_BLE_PVT_ADDRESS_TIMEOUT"? If yes, what is the event?
Thank you very much for reading the question and providing any comments or suggestions.
Best regards,
Jiabin
Show LessHello,
I'm investigating either PSoC64 family is certified FIPS 140-3 or not.
If not, please tell me type of other certified FIPS .
Please check and answer this.
Best regards,
Yuki Aikawa
Show LessHello, I have a question about the problem that occurred while creating the file 'bin' in 'Keil'.
; Cortex-M4 application flash area
LR_IROM1 FLASH_START FLASH_SIZE
{
ER_FLASH_VECTORS +0
{
* (RESET, +FIRST)
}
ER_FLASH_CODE +0 FIXED
{
* (InRoot$$Sections)
* (+RO)
}
ER_RAM_VECTORS RAM_START UNINIT
{
* (RESET_RAM, +FIRST)
}
RW_RAM_DATA +0
{
* (.cy_ramfunc)
* (+RW, +ZI)
}
; Place variables in the section that should not be initialized during the
; device startup.
RW_IRAM1 +0 UNINIT
{
* (.noinit)
}
; Application heap area (HEAP)
ARM_LIB_HEAP +0 EMPTY ((RAM_START+RAM_SIZE)-AlignExpr(ImageLimit(RW_IRAM1), 8)-STACK_SIZE)
{
}
; Stack region growing down
ARM_LIB_STACK (RAM_START+RAM_SIZE) EMPTY -STACK_SIZE
{
}
; Used for the digital signature of the secure application and the
; Bootloader SDK application. The size of the section depends on the required
; data size.
.cy_app_signature (FLASH_START + FLASH_SIZE - 256) 256
{
* (.cy_app_signature)
}
}
; Emulated EEPROM Flash area
LR_EM_EEPROM EM_EEPROM_START EM_EEPROM_SIZE
{
.cy_em_eeprom +0
{
* (.cy_em_eeprom)
}
}
Above is the contents of the 'sct' file in the ToolChain_ARM folder.
If you proceed with the build in the current situation, it will be displayed as a folder, not a file, as shown below.
If i use 'hex2bin' to switch to 'bin', the function "EM_EEPROM" will not be available.
If you look at the 'sct' code above, it seems to be caused by the load area being divided into LR_EM_EEPROM and LR_IROM1.
I want to know how to combine the areas of "LR_EM_EEPROM" and "LR_IROM1" to build.
Show Less
User | Count |
---|---|
64 | |
46 | |
13 | |
12 | |
11 |