PSoC™ 6 Forum Discussions
Hello,
we have some questions about the BLE stack.
Here are some details about our setup:
Chip: CY8CPROTO-063-BLE (CYBLE-416045-02)
Modus Toolbox: 3.1.0
BLE Stack: 3.8.0 (WICED/AIROC BLE)
1. In the default configuration, the BLE stack is used in dual-core mode, i.e. BLE controller on CM0p with predefined image CM0P_BLESS, BLE stack on CM4, and IPC for communication between the two CPU cores.
Is it possible to move the whole BLE functionality (BLE controller + BLE stack) to CM4 core, and use predefined image CM0P_SLEEP on CM0p?
I found some examples and documentation for using PSOC Creator and the old BLESS stack, but none for Modus Toolbox and the new WICED/AIROC BLE stack.
2. Is there a project implementation available, for building and modifying the CM0p image CM0P_BLESS on our own?
Hello,
I am going over this document to enable OTA for my code: https://github.com/Infineon/training-modustoolbox-level3-bluetooth/blob/master/Type1/Manual/Ch09-OTA.pdf
As a first step, I am trying to create a Modus Toolbox project by using downloaded code from https://github.com/Infineon/mtb-example-psoc6-mcuboot-basic, but I am having trouble. MTX is not recogniZing this as a project so I guess it lacks some files.
How do I kick this off?
Also I am using Bluetooth_Hello_Sensor code, which has only 1 main file (not separate for cm0p and cm4). Should the application example have separate ones to be able to follow this manual? Please advise.
Show LessHello
I am using Bosch BME680 sensor. I have also to integrate to my project the Bosch BSEC library that executes post-processing on the sensor data.
Bosch provides for the BSEC API the header files to be included and also pre-compiled static library (for ARM Cortex M4 as well as M0+) to be linked.
How can I do this in PSoC Creator ?
thanks
Show Less
Hello
I am trying to integrate pre-compiled library of Bosch BME680 sensor BSEC API. It includes 3 ".h" files and a pre-compiled ".a" file.
I followed the instructions in: https://community.infineon.com/t5/PSoC-4/PSoc-Creator-4-2-and-a-lib/td-p/149076
to integrate a pre-compiled ".a" library in PSoC Creator.
I added the links to the file and directory as shown.
Yet, I get this compilation error
I executed clean-build to make sure the changed have been updated, and yet same result of missing files.
Any clue what steps might be missing here ?
thanks
Show Less
Hola comunidad! quiero que me ayuden a adaptar los siguientes códigos (archivo .c y .h) para mi pantalla LCD con modulo I2C (PCF8574). Aun no logro tener una comunicación, es decir no logro escribir una palabra sobre la pantalla ¿Qué es lo que me estaría faltando?¿que es lo que estoy haciendo mal?. La placa que estoy utilizando es PSoC6-CY8CPROTO-062-4343W. El entorno por la cual estoy realizando el código es Eclipse IDE Modustoolbox 3.1. Adjunto dichos archivos abajo. Muchas gracias!
Show LessHello all.
I have been trying to program the CYBLE 416045-2 chipset standalone but I'm not able to do that through the evaluation board.
I have bought 10 CYBLE 416045-2 chips and one evaluation board for that. Somewhere I saw over the community forum that you can program the those chips by connecting through the J9 header that is the module SWD header. I soldered the chip onto one of the testing PCB I made and took wires and connected it to the J9 header of the evaluation board but somehow I am not able to program it standalone. Can you tell me the process to do this? It's quite urgent I'm not able to find the answer to this over the community in the past 7 months.
Thank you for your help in advance.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/PSoC-6/Programming-an-external-CYBLE-416045-2-chip-through-the-CYBLE-416045-eval-board/td-p/690221
Show Lesshi
i'm student who has a class embedded systems, we are working with modustoolbox and psoc6. i recentlly bought a new computer and now is my modustoolbox extreemly slow during the build phase. Building a simple project takes 10 minutes.
During the build the build gets stuck on the last line of this:
16:29:06 **** Build of configuration Debug for project RC_CAR ****
"C:\\Users\\quint\\ModusToolbox\\tools_3.0\\modus-shell\\bin\\make" CY_MAKE_IDE=eclipse CY_IDE_TOOLS_DIR=C:/Users/quint/ModusToolbox/tools_3.0 CY_IDE_BT_TOOLS_DIR= -j7 all
Tools Directory: C:/Users/quint/ModusToolbox/tools_3.0
Searching installed tools in progress...
Searching installed tools complete
Initializing build: mtb-example-empty-app Debug APP_CY8CPROTO-062-4343W GCC_ARM
Prebuild operations complete
Auto-discovery in progress...
Auto-discovery complete
Commencing build operations...
Tools Directory: C:/Users/quint/ModusToolbox/tools_3.0
Constructing build rules...
Build rules construction complete
==============================================================================
= Building application =
==============================================================================
Generating compilation database file...
-> ./build/compile_commands.json
at this point the build is verry slow and can take up to 10 minutes and more. After this point the build is finished in like 10 seconds. Can someone help me out??
Show LessHello all,
This is my first ever project using emwin and I'm trying to interface a TFT display from adafruit using SPI SCB and emwin graphic library on PSOC Creator IDE. So far I've found many example using the GraphicLCDintf_1 component but none with serial, so I'm getting kinda desperate. I'm still pretty green to PSOC creator, so if anyone can take a look at my project and point me in the right direction then that would be great.
Thank you so much
Phong
Show Less