Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

riteshEB
PSoC™ 6
I am evaluating mtb-example-psoc6-switching-power-modes example on CY8CKIT-062S2-43012. Power is applied via Kitprog3 USB connector and I am measuring... Show More
skrovvidi
PSoC™ 6
My device is bus powered when connected to the host and battery powered ( self powered ) when not connected to host Is it possible to use the USB DP p... Show More
SimonCanada
PSoC™ 6
I am using a PSoC 6 BLE Pioneer board, Creator 4.4 with PDL 3.1.5 with some custom CapSense sensors connected to P8 and 9. Target device has a very li... Show More
ele
PSoC™ 6
I am currently experiencing a problem with the system operation of ModusToolbox version 4.4 and a CY8CKIT-062-WIFI-BT kit. After creating an applicati... Show More
GrCa_1363456
PSoC™ 6
What modification are needed to the Code, MakeFile or Libraries such that the compiler doesn't attempt to utilize CRYPTO or TRNG features that don't e... Show More
Communication
PSoC™ 6
Hello!I am having problem reading DHT11 sensor and sending data to mobile app using PSoC 063 BLE Prototyping kit and Modus Toolbox software, when read... Show More
podericof
PSoC™ 6
Hi there, I'm using PSoC Creator 4.4 with PDL 3.1.1. When I try to debug the CM4 I have the following error: The start request failed. Encountered err... Show More
notAnumber
PSoC™ 6
Hello!I am trying to setup a watchdog timer on my PSoC 6 board, CY8PROTO-062-4343W. This using the cy_pdl.h library. I followed the steps in the PSoC ... Show More
Nirmith
PSoC™ 6
Hi  I need to know can we bootup the MCU using external memory for booting up the system. If yes can you suggest me a part compatible with CYB0644ABZI... Show More
rushikeshmunde
PSoC™ 6
Hi,  I am used PSoC 6 PROTO Kit & I have initialized tcpwm counter using Device Configurator.  I want to use it as interval timer,  when I run it on C... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.