PSoC™ 6 Forum Discussions
[Infineon PSOC 62S4 PIONEER KIT evaluation] - preparatory work
First, find the download link of ModusToolbox™ software on our official website https://www.infineon.com/cms/cn/design-support/tools/sdk/modustoolbox-software/, select the corresponding version number and operating system, and download it. If you use the Windows system, you don’t need to install other applications, but if you use other systems, you need to install different applications according to your needs.
When installing, we should pay attention. If it is not installed in the default location, you need to set the environment variable CY_TOOLS_PATHS to point to your actual installation path, as shown in Figure 1. Note that '/' should be used. At the same time, the Makefile in the project file needs to be modified accordingly: CY_TOOLS_PATHS+=F:/ModusToolbox/tools_3.0. Readers can read the ModusToolbox™ tools package installation guide file to set other environment variables by themselves.
Figure 1 Setting the environment variable CY_TOOLS_PATHS
Click new application to enter the interface shown in Figure 2. This is because we need to fetch resources from GitHub. We can access GitHub by using something like a proxy link. Here we use other methods to download the appropriate version of ModusToolbox™ Offline Libraries, the link is as follows https://softwaretools.infineon.com/tools/com.ifx.tb.tool.modustoolboxofflinecontentpackage.
After the download is complete, under the Windows system, you need to use cmd to create a .modustoolbox folder, find the installation directory, and then use the mkdir .modustoolbox command. After the setting is complete, on the choose board support package interface, select setting->offline.
Figure 2 choose board support package interface
Enter the page in Figure 3 and select the corresponding one.
Figure 3 choose board support package interface
Editor: perceptive-ic
Show Lesshi,
For our custom board using following chip CY8C6245LQI-S3D42, I have following requirement.
1) USB CDC based DFU.
2) The application should also have a USB CDC.
3) I want a utility to send the updated cyacd file from a arm based linux platform to DFU.
Do you have any working example or any process to create it.
Regards,
Madhav
Show LessHi,
we are trying to send data to the SQL server using CY8CPROTO-062-4343W PSOC6 WIFI-BT PROTOTYPING KIT. We had used Web server code and key_ch04b_ex06_httpbin_post code . when code got downloaded , WIFI is getting connected successfully through via HTTP webpage. After we are trying send post request to SQL server that time the request is not getting send .could you please help me to sort out this issue. What are the possible requirements that we have to take to implementing this project
Show Less
Hi,
We plan to power VBACKUP signal on with a supercap (which is charged via 100 ohm resistor) on a project using PSOC6 (running at 3V).
It appears that while the supercap is charging the UART on P0 voltages are low as a result we can't communicate with the device on the initial power up. Although, its only a minute or so, but it affects our production testing.
My understanding was that backup domain would use VBACKUP or VDDd (which ever is higher), where VDDd is set to 3V.
When calling Cy_SysPm_BackupGetSupply(), it returns CY_SYSPM_VDDBACKUP_DEFAULT (which should have selected VDDd if it is present).
Am I missing something else in the configuration?
Show Less
Dear colleague,
I am working on a project where I am using the CY8CKIT - 062 PIONEER KIT , my project is versioned and every thing is working fine ( compilation, libraries, BSP ..) , until I changed my laptop.
I pulled the project from the server to continue working on ( knowing that I re-generate the mtb_shared libs using the library manager) and just after that the problem of the 'unresolved inclusion' starts. I tried to fix this using the indexer update and so on but nothing is useful!
An other think that I want to mention here, is that when I create a new project based on the 'empty project template' the same problem occurs.
Thank you for your help .
Reagrds,
Show Less
Hi,
I'm working on a project with the region cy_em_eeprom is on CM0p because BLE is on this core.
I want to access the same region from CM4 to fix a production defects writing ble data from CM4.
Is that possible and how?
Thanks
Show LessHi Myself HEMANTH,
Currently I'm working on PSOC6 Evaluation board. Actually we have project on REVERSE OSMOSIS WATER PURIFIER by SIM Chip rechargeable and data also we need to store by using EEPROM with wifi configuration will connect our eval board through our main hardware board codes need to flash and store the data and that data need to send cloud server(
main server) by using PHP Server for that we have dashboard of domain in that we need to operate.
with is project shall anyone knows means just ping me i will contact you can help us.
Our Basic details
PSOC6 Bsps
CY8CPROTO-062-4343W
IC:- CY8C624ABZI-S2D44
Radio chip: LBEE5KL1DX (CYW4343WKUBG)
Flow meter
These are we are using basic components
if anything need to ask please contact us:
mail id:- hemanthpappu831@gmail.com
Thanks & regards
Hemanth pappu
Show LessHi All,
I'm using CYW43455 chip for Wi-Fi support. Here I'm using Wi-Fi enterprise feature but, while using this not able to connect with radius server using specific routers(i.e. TP-Link, D-Link).
Same scenario I tried with Cisco router & able to establish connection properly. If anyone knows regarding this issue please, let me know.
FYI :Referring WICED-Studio-6.6 code for development
Thanks
Show Less