PSoC™ 6 Forum Discussions
Hi Myself HEMANTH,
Currently I'm working on PSOC6 Evaluation board. Actually we have project on REVERSE OSMOSIS WATER PURIFIER by SIM Chip rechargeable and data also we need to store by using EEPROM with wifi configuration will connect our eval board through our main hardware board codes need to flash and store the data and that data need to send cloud server(
main server) by using PHP Server for that we have dashboard of domain in that we need to operate.
with is project shall anyone knows means just ping me i will contact you can help us.
Our Basic details
PSOC6 Bsps
CY8CPROTO-062-4343W
IC:- CY8C624ABZI-S2D44
Radio chip: LBEE5KL1DX (CYW4343WKUBG)
Flow meter
These are we are using basic components
if anything need to ask please contact us:
mail id:- hemanthpappu831@gmail.com
Thanks & regards
Hemanth pappu
Show LessHi All,
I'm using CYW43455 chip for Wi-Fi support. Here I'm using Wi-Fi enterprise feature but, while using this not able to connect with radius server using specific routers(i.e. TP-Link, D-Link).
Same scenario I tried with Cisco router & able to establish connection properly. If anyone knows regarding this issue please, let me know.
FYI :Referring WICED-Studio-6.6 code for development
Thanks
Show LessHi everyone,
I'm working with the Cypress PSoC 6 board in Mbed OS. I need to develop an AP Mode WiFi example. Are there any examples available? Can you send me some resources to get started?
Thank you.
Show Less1. which development IDE is a good future and which IDE is easier to learn for PSoC 6 MCUs?
2. how many ways can we flash the code for Psoc 6 mcus?
3. How many IDEs are available in the market for developing code for PSoC 6 MCUs?
Show LessHi ,
I am running a PSOC6 USB HID Generic setup , The code works from the IMO clock trimmed to USB mode.
The problem I am currently experiencing is when everything is run from the IMO clock at 96Mhz (because it can't go higher 😞 ) the HID enumerates and I can send data . However, switching this to the external TCXO gives me much more accuracy and a potential for higher core clocks the HID side does not work anymore although the paths in the Device configurator and dividers are set up correctly .
I principal the initial sources are the only side that changes , so it should not affect the USB enumeration
Below is 4 scenarios on this 2 working and 2 not working. in order to increase the CORE clock I need everything to run from the EXTCLK . The cores need to be CM4 150Mhz and the CM0 75Mhz , as it is right now this is not possible.
IMO working config below
EXTCLK NOT working 1
Extclk NOT working2
Extclk working 2
Any assistance is welcome.
Regards
C
Show Less
Hi all
The example: Adding TFT to my project - Infineon Developer Community
I have a question about my project being built in MTB. I'm following the example of using the CY8CKIT-028-TFT on the CY8CKIT-062-WIFI-BT. However instead of that board I'm using the CY8CKIT-062-BLE (the example uses WIFI-BT), but the TFT shield is compatible with both
When I plug my board in and click program (using kitprog3 miniprog4) the screen doesn't appear to display anything. I followed all the steps and ensured I'm using the right BSP for me. No errors are produced on running but i do get this output:
I'm not changing any other settings, I'm following the tutorial, putting the lines of code in and pressing program so not sure if thats where im going wrong
Any ideas?
Kind regards
Show LessSo am trying to debug the program by adding the breakpoints and am getting this error. What does this error means and how can we resolve it?
Info : SWD DPIDR 0x6ba02477
Error: Failed to read memory at 0xfffff000
Info : SWD DPIDR 0x6ba02477
Error: Failed to read memory at 0xfffff000
Info : SWD DPIDR 0x6ba02477
Hi all,
I want to simulate some basic assembly language code so I understand Arm assembly language better. What I have in mind is very basic. I'm by no means trying to have an actual project. I'll just have a few assembly language instruction do stuff and see how the cpu register change value. I'm pretty sure there is stuff (code) that needs to setup some basic stuff before I can write my code. I'll be using the debugger to step thru my assembly code and look at the cpu registers. How do I go about making a very very basic project in assembly code so I can do this? A simulator for the CM4 would work too but what comes up after a google search doesn't seem to be for the CM4... and I have a perfectly working CM0p/CM4 CPUs right here 😁.
Thanks
Show Less