Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

skruglewicz
PSoC™ 6
I would like to create a library  to be used to connect to an external sensor using a PSoC 6 board that is supported in ModusToolbox. I have two board... Show More
hunter
PSoC™ 6
IDE:Modustoolbox 3.1 Lib:PDL(Generated using the device configurator)   Clock:16bit Clk,Source Clock 100Mhz,Divider 109   The target baud rate is 1152... Show More
heike
PSoC™ 6
Hi, is there a possibility to cross compile and flash an application which uses mtb-hal library without Modustoolbox for PSoC? Or at least disable aut... Show More
Manoj_Kumar
PSoC™ 6
I want to write and read the data transmitted through RS485. Am using CY8C6245LQI-S3D72 BSP.  But the issue arises when am trying to read the data, bu... Show More
yanqil
PSoC™ 6

Digikey shows the miniprog 4 - CY8CKIT-005 is obsolete.  What is the replacement for this part?

Thank you.

WolfgangCS
PSoC™ 6
I am currently using a PSoC3 CY8C3246PVI-147 and would like to upgrade to PSoC6 CY8C6347BZI-BLD33. Regardless of the hardware details regarding the PC... Show More
StanGibson
PSoC™ 6
I have installed and reinstalled Modustoolbox 3.1 and cannot get any example project to build.  This is likely my inexperience, but each time I try to... Show More
EyLa_1625036
PSoC™ 6
Hello all , I want to build a custom pcb ,and i was wondering  what are some practical uses for a QSPI flash that is connected to the psoc6 device ? I... Show More
YongseokJeon
PSoC™ 6
Hi,I'm testing with the example below.- CY8CKIT-062-WIFI-BT, Dual-CPU_IPC_Semaphore After build, the app_combined.hex file is created in the Dual-CPU_... Show More
asacharya
PSoC™ 6
Hi, I wanted to know the hardware differences between pSoC32 and pSoC64.  I have a custom designed board from customer with psoc62.  I wanted to redes... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.