Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

dhruv1997
PSoC™ 6
Hi PSOC62 Team, I have written the custom OTA application on CY8CKIT-02S2-43012 by using MCUBoot library. Now my requirement is , I need to port entir... Show More
SagginDragon
PSoC™ 6
 We're basing our code on the examples in the documentation but seem to be unable to get an actual reading off the ADC. Debugging has traced the probl... Show More
peya_1337906
PSoC™ 6
Hi , I use MTB3.0 to compile "QSPI_XIP" project , show out the follow error message:  : fatal error: cannot execute 'cc1': CreateProcess: No such fil... Show More
Komugiz_King
PSoC™ 6
Dear forum members, I'm currently working on a project using the CY8C6347BZI-BLD53 board from Cypress Semiconductor, and I would like to integrate a "... Show More
l_diserio
PSoC™ 6
Hello,   I'm using CY8CPROTO-063-BLE PSoC 6 PROTOTYPING KIT with CYBLE-416045-0243-SMT which is used for reading the position of a motor with an encod... Show More
GrCa_1363456
PSoC™ 6
Precision Illumination Signal Modulation (PrISM) is a differentiating feature supported by Infineon. There are components and code examples for PrISM ... Show More
Atsumin7110
PSoC™ 6
Description I am using CYBLE-416045-02 and I am trying to make the MCU to enter deep sleep while the BLE controller embedded in the MCU is enabled. Ho... Show More
Manoj_Kumar
PSoC™ 6
I am trying to check if wdt reset works, but unfortunately its not. In the code am blinking blue led (P7_3) whenever a reset occurs because of user re... Show More
Manoj_Kumar
PSoC™ 6
I am trying to check if wdt reset works, but unfortunately its not. In the code am blinking blue led (P7_3) whenever a reset occurs because of user re... Show More
krishvazirani
PSoC™ 6
Hi, I am looking to purchase a bulk order of the PSOC 6 but before I do, I wanted to know if there are any tinyML benchmarking results that are out fo... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.