PSoC™ 6 Forum Discussions
text.format{('custom.tabs.no.results')}
I am trying to update the stored data into the EEPROM storage. Am using
Dears,
I am having an issue to limiting the radar distance in Radar Presence detection code and it is limited to the 0.66 meters at least but in my project I need it to be 0.2 meters at most. I connected my kit to the computer via usb cable and I want to check it in Radar Fusion GUI but when I openned the app it says no connection found. When I tried to add manually I can not select the board or anything else.Can anyone help me in this situation? How can I fix that limit problem and GUI problem.
Best regards,
Eray
Show LessI'm trying to use the number of enabled ADC channels to set the length of an array that will store the voltage readings from the ADC (to be written with a for loop) for use later in the program. It looks like the variable I want to call is chanEn as shown here:
const cy_stc_sar_config_t BusVoltage_config =
{
// snip rest
.chanEn = 1UL,
// snip rest
}
I ought to be able to call BusVoltage_config.chanEn as the array length (trying to do it this way for code portability's sake), but testing it with different "Number of Channels" values on the parameters tab is giving odd results: 1 enabled channel sets chanEn to 1UL, 2 sets it to 3UL, 3 sets it to 7UL.
Is there an easy way to dynamically set this array length? Is chanEn maybe set by a formula that I can invert to get the flat quantity of enabled channels?
Show LessHello,
I'm using CYB0644ABZI-S2D44 on a costume board with modustoolbox 3.1.
The UART Tx & Rx pins are swapped... (p3.1 & p3.0)
Is there a way to swap them back?
Thank you,
Dvir
Show LessHello,
I am looking at the PDL documentation for SDHC under the "Assign and Configure Pins" section. The PDL documentation suggests "Also, the SD Host pins must be configured in Strong Drive, Input buffer on:" My question is as follows:
Is there some PSoC6 SDHC limitation or some other general hardware reason why we must use Strong Drive? What if we do not want to install external pull up resistors on our board and wish to use the PULLUP mode of the pins instead? Why does the documentation insist on Strong Drive must be the mode?
Show Less
can we create library for psoc6 with some c code and UART.
i have c function and wanted to create a library file to use in with other project how can i create.
mean,
ill receive some data in serial port based on that i wanted to trigger led and then reply back on serial.
this i wanted use has a library in other project.
please do suggest.
Show LessHello, my design is not working as expected. The task is just reading out the resistance change of pressure sensor. I've finished the coding part, but I don't know what's the problem with my codes. Please someone takes a short glance.
Show LessHello, I created a project for reading out multiple sensors' resistances. But it seems like reading out the same sensor among 16 sensors every time. I've checked the codes and I'm thinking there's nothing wrong from my side. It seems like Cy_GPIO_write() doesn't even work during the loop.
Show LessHello, I'm a beginner in Microcontroller, especially Psoc. I want to build a AMux Seq to select channel for ADC further measuring Voltage. But I cannot build the application. Can anybody tell me where is the Problem?
Show Less