Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

Caloripher
PSoC™ 6
Dears, I am having an issue to limiting the radar distance in Radar Presence detection code and it is limited to the 0.66 meters at least but in my pr... Show More
SagginDragon
PSoC™ 6
I'm trying to use the number of enabled ADC channels to set the length of an array that will store the voltage readings from the ADC (to be written wi... Show More
dvirbuc
PSoC™ 6
Hello, I'm using CYB0644ABZI-S2D44  on a costume board with modustoolbox 3.1.  The UART Tx & Rx pins are swapped... (p3.1 & p3.0) Is there a way to sw... Show More
WeGa_288606
PSoC™ 6
Hello,  I am looking at the PDL documentation for SDHC under the "Assign and Configure Pins" section. The PDL documentation suggests "Also, the SD Hos... Show More
Amar_Hiremath
PSoC™ 6
can we create library for psoc6 with some c code and UART. i have c function and wanted to create a library file to use in with other project how can ... Show More
markolloss
PSoC™ 6

Test

Sun08
PSoC™ 6
Hello, my design is not working as expected. The task is just reading out the resistance change of pressure sensor. I've finished the coding part, but... Show More
Sun08
PSoC™ 6
Hello, I created a project for reading out multiple sensors' resistances. But it seems like reading out the same sensor among 16 sensors every time. I... Show More
Sun08
PSoC™ 6
Hello, I'm a beginner in Microcontroller, especially Psoc. I want to build a AMux Seq to select channel for ADC further measuring Voltage. But I canno... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.