Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

gaohailong
PSoC™ 6

CY8C62XA芯片IO口耐受电压是多少、能到5V吗?从哪个地方可以查的到 谢谢

gaohailong
PSoC™ 6
CY8C62XA芯片IO口耐受电压是多少、能到5V吗?从哪个地方可以查的到 谢谢
Sreehari
PSoC™ 6
In modus tool I am open PSoC6 in that I open empty app and tried to build. While building time time it is success but while coming to debug time some ... Show More
htn
PSoC™ 6
I am trying to a program that sets the value obtained from the ADC to a control register via DMA. I have looked into it myself and tried my best, but ... Show More
Manoj_Kumar
PSoC™ 6
I am trying to update the stored data into the EEPROM storage. Am using  InitializeAndReadEEPROM() to initialize and enter some data into the storage... Show More
Caloripher
PSoC™ 6
Dears, I am having an issue to limiting the radar distance in Radar Presence detection code and it is limited to the 0.66 meters at least but in my pr... Show More
SagginDragon
PSoC™ 6
I'm trying to use the number of enabled ADC channels to set the length of an array that will store the voltage readings from the ADC (to be written wi... Show More
dvirbuc
PSoC™ 6
Hello, I'm using CYB0644ABZI-S2D44  on a costume board with modustoolbox 3.1.  The UART Tx & Rx pins are swapped... (p3.1 & p3.0) Is there a way to sw... Show More
WeGa_288606
PSoC™ 6
Hello,  I am looking at the PDL documentation for SDHC under the "Assign and Configure Pins" section. The PDL documentation suggests "Also, the SD Hos... Show More
Amar_Hiremath
PSoC™ 6
can we create library for psoc6 with some c code and UART. i have c function and wanted to create a library file to use in with other project how can ... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.