Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

asacharya
PSoC™ 6
Hi, I could see for cy8cproto-064b0s3 there is a prototype board - link below. https://in.rsdelivers.com/product/infineon/cy8cproto-064b0s3/infineon-psoc-64-secure-boot-prototyping-kit-psoc/2414257?srsltid=ASuE1wQpQS8slXQk9fnQWLUfG77KeszvEJ6QatrlBo7ziJ3urlQLNN7TPQE... Show More
air
PSoC™ 6
Hello.   I am using CY8C6247. I am trying to write data to the auxiliary region using the EM_EEPROM library.   M0 enables M4 and does nothing. I am wr... Show More
OnyancoTama
PSoC™ 6
Hello. I'm beginner for PSoC series and this is my first post. I use PSoC63BLE and ModusToolbox as IDE . I don't use PDL but use HAL in my program fro... Show More
shiyouxue
PSoC™ 6
Dear Forum  :  We developed our  embedded software with PSoC6. But we encountered the following problem:In some boards,PSoC6 can't wake up from deep s... Show More
SagginDragon
PSoC™ 6
The saga continues lol. We've got our Em_EEPROM working, but I have a row addressing question regarding Cy_Em_EEPROM_Write(). It's recording single da... Show More
gaohailong
PSoC™ 6
在eclipse中导入多核工程后点击编译,提示Libraries: "core-make recipe-make" not found. Run "make getlibs" to ensure all required build and code dependencies are present... Show More
gaohailong
PSoC™ 6
使用PSOC6芯片,由于M0核内存不够,我把mo核内存调成32k,对应m4核内存做相应的偏移,就不能对m4核仿真了,但是M0核能够正常仿真,我把M4核内存分配改成默认值就可以仿真了,使用的 是J-LINK调试器,恳请各位高手给与指导   先跪拜了  谢谢 Show More
Sturla22
PSoC™ 6
Hello, I have configured an SRAM chip to work with SMIF in normal mode. Now I want to enable XIP/memory mapping of that memory. It seems like the memo... Show More
jay_li
PSoC™ 6

Hi all,

XENSIVTM MEMS microphones PDM接口搭配MCU推荐哪个型号?

是否可以直接处理识别PDM讯号?

 

 

Tim_Shih
PSoC™ 6
Dear Receiver, We know there are many kinds of power supply source in PSoC 6.  For example: there are VDDD, VDDIO1, VDDIO2, VDDA, etc. As I know, the ... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.