Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

victor2022
PSoC™ 6
HI, what happened when I call cy_retarget_io_init() and returned error? The source code is as the following: #define CYBSP_DEBUG_UART_TX P5_1_SCB5_UAR... Show More
matthiasb
PSoC™ 6
Hey, I'm trying to build a project which is based on a modified "Security Example"  Project. I want to use the btstack, so  deleted the CM0+ project a... Show More
srini_a
PSoC™ 6
Hello Community, I'm trying to interface the WM8940 speaker with PSoC 62. Is there a driver /example available for this? I see one is available for WM... Show More
jimharris
PSoC™ 6
I am looking for DFU code example using XIP to store/execute App1. I am using ModusToolBox 3.0. Also using the PSoC 6 BLE Pioneer Kit CY8CKIT-062-BLE.... Show More
Tim_Shih
PSoC™ 6
Dear Receiver, We know all documents which talk about secure boot is based on PSoC 62, 63 or 64. Because the secure boot mechanism includes M0+ and M4... Show More
Sachin_Patel
PSoC™ 6
I working on a project where I have to transfer data periodically over SPI in DMA mode. To avoid CPU intervention I want to trigger SPI DMA transfer u... Show More
Translation_Bot
PSoC™ 6
I have tried to get a count using psoc63-ble but it does not work.When I tried to take counts at 10MHz I could only take counts in the lower frequency... Show More
DuS
PSoC™ 6
Customer faced issue to install the CY8CPROTO-063-BLE Evaluation Board in Windows 7.  User followed the below document instruction from page 19-page 2... Show More
IronWaffle
PSoC™ 6
Good day! I am working with the CY8CPROTO-062-4343W microcontroller and using the Infineon/abstraction_rtos library for an application. For porting, a... Show More
Hemanth1
PSoC™ 6
Hi, We are facing issue with New EEPROM IC  chip in PSOC6 Hardware board. We need to sort-out that issue getting error in output write section write f... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.