PSoC™ 6 Forum Discussions
I'm anxious to start playing with PSOC 6 so I hate to ask because I know the answers are inevitably optimistically biased, but, what's the ETA for PSOC 6 DVK's? I promise not to hold anyone's feet to the fire, just trying to understand if we're talking about the next few weeks, next few quarters or next few years?
Show LessHi,
PSoC6 BLE looks very exciting and a huge step up from PSoC4 on so many levels.
Are there plans for EzBLE modlues, and if so in what sort of timeframe?
BLE regulation and qualification is a huge hurdle for SME and Maker type innovators.
Regards Zig
Show LessI am working on PSOC4 BLE at present. I want to switch to PSOC6 and had some queries listed below:
1. Whether PSOC6 will work with PSOC creator 4.1, If not than which IDE is available for PSOC 6.
2. Whether MiniProg3 Programmer/Debugger can be used with PSOC6.
3. Whether ready made Bbluetooth stack is available for BLE 5 in PSOC 6.
Show LessCan someone describe the timer peripherals that are available to run in Deep-Sleep? How many are there, and how many are consumed by the BLE stack?
Show LessHello,
I am looking for the docs for the new PSoC6.
Can somebody provide me with the links to get the proper version of Creator, PDL etc.? These don't seem to be current published.
I believe I need:
+ Creator 4.1 (I have 4.0)
+ PDL (3.0), etc.
+ QuickStart Guide
+ Code Examples
+ Any other useful links, noob resources
Regards,
Bryce
Show LessHi, I hava a question. Is there an example of using TEE?
According to some rumors on the other PSoC forums, it sounds like the new PSoC 6 chip has support for multiple bluetooth connections simultaneously. For example, two peripherals connected to one central sending notifications (limited by connection settings obviously).
Has anyone tested/can confirm this?
Show LessI have tried to implement the interrupt on PSoC6 BLE pioneer kit, but the interrupt of PWM is not occurred. I confirmed GPIO interrupt occurred.
I attach my sample project as a reference.
My questions are:
a) What is needed to occur the interrupt?
a-1) Is the configuration of PWM correct?
b) What is the API to clear the interrupt flag? I can't find it.
Please let me know.
Show LessWhere can I find information about the bluetooth stack? Is the bluetooth stack offered tied to a certain RTOS? If I have to use my custom RTOS along with the bluetooth stack provided, is that possible?
Show Less