Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

ChRe_4711096
PSoC™ 6
The attached project uses DMA to retrieve the channel currently handled by SARSEQ. This is done by DMAing SAR_STATUS into a control register on every ... Show More
jihe_298791
PSoC™ 6
How do you write a UART receiver ISR in FreeRTOS when I send a command and sometimes get a response quickly. I'm trying to use a binary semaphore but ... Show More
Zion
PSoC™ 6
hi,我有购买一套“ CY8CKIT-062-BLE PSoC 6 BLE Pioneer Kit”,配套的capsense的代码是基free os的参考代码,我现在想单独学习capsense功能,单独建立了一个不跑OS的capsense工程,基本与基于free os的参考代码一致,只是没有使用Fr... Show More
ChRe_4711096
PSoC™ 6
I'd like to sneak in a temperature measurement from time to time, while the ADC is usually busy scanning 4 differential channels using SARSEQ. From th... Show More
MuNa_4652896
PSoC™ 6
Hi again.I have been testing the connection between both the Dongle and the Psoc 6 Kit. It seems I am only limited to send 20 bytes per notification p... Show More
AlSt_3233956
PSoC™ 6
Hello,using PSoC Creator 4.3 with PDL v3 = 3.1.2 and PDL v2 = 2.1.0. The BLE Device is configured as Peripheral the connection settings are the follow... Show More
GeGa_1196981
PSoC™ 6
I Have a question regarding the PSOC6 as central modeWhat I want is to read the nerby devices but I can't find an example that works on psoc 6I tried ... Show More
ScKi_1600301
PSoC™ 6
I have a simple program for reading the JEDEC information from a serial flash chip using the low-level API.static void SPI_FlashWriteByte(uint8_t byte... Show More
WiWi_4702256
PSoC™ 6
I need to be absolutely certain of the following: My hardware engineer asked me to verify:P10_0 can be configured A to DP11_2 thru P11_6 can be config... Show More
ChRe_4711096
PSoC™ 6
I'm looking for ways to ease the chip from some combinatorial logic. I have 4 instances of a component that has a 4-input OR gate, and I'm tempted to ... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.