PSoC™ 6 Forum Discussions
Here I have set up a matrix button who has 5 rows and 5 columns that make up a total of 25 sensors. But I only see 10 Sensor element IDs in CapSense_Configuration.h. I want to save the Rawcount of the 25 sensors in a parameter like "Value", how do I write this code?
I used this code for storage when I had a single button before, but now I only have 0u to 9u instead of 0u to 24u.
uint16 val0 = CapSense_dsRam.snsList.button0[0u].raw[0u];
Show LessHow do I use Jlink (SEGGER) to read and write via SWD? JLink has not found a CYPD6125 signal, nor has the official FLM or xml file corresponding to CYPD6125 been found
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/PSoC-6/CCG6-CYPD6125-40LQXIT/td-p/641815
Show LessBoard: CY8CPROTO-062S2-43439
ModusToolbox : v3.1
Example BSP code: ADC basics
----------------------------------------------------
Error Snippet::
Info : kitprog3: acquiring the device (mode: reset)...
Error: kitprog3: failed to acquire the device
Info : clock speed 2000 kHz
Error: Error connecting DP: cannot read IDR
Error: Error connecting DP: cannot read IDR
Error: Error connecting DP: cannot read IDR
Error: DAP 'psoc6.cpu' initialization failed (check connection, power, transport, DAP is enabled etc.)
Info : psoc6.dap: powering down debug domain...
Error: Error connecting DP: cannot read IDR
Error: Error connecting DP: cannot read IDR
I want to test the PSoC® 6 BLE.
Are PSoC™ Creator, PSoC™ Designer and PSoC™ Programmer free or commercial?Hey guys,
I used Capsense self-cap to made a force sensor (sandwich structure), on electrode pad as the self-cap pad, another one connected to the GND. It works very good, but now I wanna make a 5x5 sensor array, so I set 5 Buttons(0~4) in CSD (self-cap), and a MUX for other 5 GND Pins.
So I used this code:
But the problem is, I can not just use "uint16 Value0 = CapSense_dsRam.snsList.button0[0u].raw[0u];" to save the data now, cause I just have 0u, 1u, 2u, 3u, 4u, but I need read out 25 data.
If I use Mutual-Cap then I can set 5TX and 5RX, then I can get 0u to 24u. But what should I do with Self-Cap?
Show Less
I have followed several different posts and tutorials about creating a custom BSP but I'm getting the following error when trying to build the BSP, both from within the ModusToolbox (3.1) as well as from the command line (the following is from the command line attempt):
make bsp TARGET_GEN=my-bsp DEVICE_GEN=CY8C6136BZI-F14
Tools Directory: /home/test/ModusToolbox/tools_3.1
Removing .mtbqueryapi file...
Searching installed tools in progress...
Searching installed tools complete
../mtb_shared/core-make/release-v3.2.2/make/core/core_utils.mk:109: *** Make bsp target is no longer supported. Use BSP assistant tool instead.. Stop.
This was executed from top-level project directory. I followed the installation guide for the ModusToolbox and believe that I completed all the steps. Could someone shed some light on why this is happening?
Show LessHi, friends,
I used ModuxToobox version 3.0.0, after I setup QSPI Configurator 4.0, I still have compiling errors as "cy_serial_flash_qspi.h: No such file or directory".
It seems that the serial-flash library has not been setup. However Usage of Quad SPI (QSPI)/Serial Memory Interface (SMIF) in PSoC™ 6 MCU (infineon.com) is under Library Manager 1.0, and I am using Library Manager 2.0, I cannot find serial-flash library under manager 2.0.
Thanks in advance.
Victor
Show LessDears,
My customer wants to develop a GUI to program firmware through miniprog4.
It has the same functionality as Cypress Programmer, but customer wants to add the features they need.
Is there any document we can refer to for this?
To make development easier, he would like to use the .dll files used by cypress programmer.
Thanks and Regards,
YS
I am using PSoC Creator to configure a counter in one-shot mode. I have a CY8CPROTO-063-BLE board. The target device is CYBLE-416045-02. How do I configure the following? On the falling edge of the button on P0[4], a counter outputs 10 cycles of a 1kHz input clock on pin P6[3]. After these 10 cycles, pin P6[3] stays low, the counter resets. The system waits for the next falling edge of the button input, starting the process over again. I would prefer a solution that configures the counter mainly through the configuration GUI.
Show LessI want to download programs using cyprogrammer, but the UI interface is gray and cannot be linked. I used a different connector. Should I use the specified connector, such as Kitprog3
Show Less