Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

GrCa_1363456
PSoC™ 6
Infineon has publicly stated PSoC 3 is produced on 130nm process. PSoC 6 is produced on 40nm process Will future PSoCs use a smaller process? What p... Show More
HYUNGWOO-YOON
PSoC™ 6
Error: kitprog3: failed to acquire the device Info : clock speed 2000 kHz Error: Error connecting DP: cannot read IDR Error: Error connecting DP: ca... Show More
Translation_Bot
PSoC™ 6
my board is CYW20829 When I was writing my BLE program based on RTOS, I created some other tasks and ran the program, which caused Bluetooth to fail t... Show More
Translation_Bot
PSoC™ 6
Hi: When I use MiniProg4 to burn in CY8C6247FD1-D02, PSOC Programmer prompts: Hex File parsing failure. Unknown record type. May I ask what causes thi... Show More
shiyouxue
PSoC™ 6
Dear forum:I write hex file to flash by cypress programmer.I can write the hex file normally, but when I open the cypress programmer, but why the Chip... Show More
rxm
PSoC™ 6
Hi, we are using a PSoC63 (on a CYBLE-416045-02 module) and are facing the following challenge: We need to pull a an output (Port 9.5) constantly low,... Show More
TW_Chia
PSoC™ 6
I am using CYBLE416045-02. I have used the example code PSoC6DfuBleApp001.cydsn and PSoC6DfuBleApp011.cydsn to add the bootload application to my appl... Show More
Translation_Bot
PSoC™ 6
Current Sampling Circuit Design Guidelines in Brushless Motor Drivers forum?smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/PSoC-6/%E6%97%A0%E5%88%B7%E7%94... Show More
LeonH
PSoC™ 6
Hi Sir, When I use "ADC basic" example with CY8CKIT-062S4, and modify the code to single end, then everything is fine, ADC is working. After I changin... Show More
Jiabin
PSoC™ 6
Hello, I am developing a BLE peripheral device based on the code example. The firmware is running in FreeRTOS, and low-power approaches are implemente... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.