Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

MiladMrad
PSoC™ 6
Hi. I'm using  cyhal_spi_transfer(cyhal_spi_t *obj, const uint8_t *tx, size_t tx_length, uint8_t *rx, size_t rx_length, uint8_t write_fill) function t... Show More
rt54321
PSoC™ 6
I am using the CY8CPROTO-063-BLE kit for a motor control application.  This kit has the built-in debugger on it. If I use the debug utility in PSOC Cr... Show More
thekbhgames
PSoC™ 6
I'm working on a project using the XMC4800 microcontroller. What are some best practices for optimizing power consumption?"   by Kat Williamson 📢 Show More
MiladMrad
PSoC™ 6
Hi. I used PSoC creator before to generate code for peripherals before and now I'm trying to migrate to modus toolbox as I've seen the answer to many ... Show More
MiladMrad
PSoC™ 6
Hi. Can someone please explain to me that by who the code for cortex M0 is generated? I remember that in PSoC creator, there were two main files for e... Show More
lppd
PSoC™ 6

触摸板手指触摸,信号下降一般有什么可能呢

Translation_Bot
PSoC™ 6
spi+dma
solved msg Solved
@Len_CONSULTRON Solved: Re: PSOC6 UDB implements four data lines and one clock line to send data is not QSPI - Infineon Developer Community   Can Oka... Show More
amin
PSoC™ 6
Hi I am using a MiniProg4 as an I2C bridge (through 12 pin) and a PSoC programmer (through 5 pin port). I am developing a code in Python, to control b... Show More
Gio0_1
PSoC™ 6
Hello guys, (EDIT down) You were helping me with other topics and I appreciate it! I want to tell you that I was working on my Project normally, and a... Show More
rt54321
PSoC™ 6
Greetings!  Using a PSOC6 with PSOC Creator 4.4.  Currently, I have a Scan_ADC that is triggered at 20kHz by a PWM timer.  When triggered, the Scan_AD... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.