PSoC™ 6 Forum Discussions
So I'm going to work on a project, where me and some friends need a bluetooth device where we connect a smartphone appplication and a remote to this device, through bluetooth connection. Here my question is: How many connection does the PSoC 63 take at the same time? I need minimum 2 connected at the same time. The only thing i found was maybe a max of 4?, but i just want to make sure.
Show LessHi,
I am using the example CE220060 - Watchdog Timer and trying to move the code from M4 to M0. It works on M4 but however not on M0. The watchdog timer interrupt handler was never called on M0. The attached is the example with simple modification of moving M4 code to M0. Are there any other settings required that I have missed in my example? Thanks!
Show LessThe latest version I see is V2.20 in PSoC Creator. Is there a newer version with Simple Mode which doesn't use 2x the amount of flash requested as stated in this post 1 year ago?
PSOC 63 Emulated EEPROM confusion - size restrictions, overhead?
Show LessIs Version UART 2.5 Component available for PSoC 6? I don't see it. I would like to use the SCB UART for Half-Duplex.
Using CY8CKIT-062-WiFi-BT with PSoC Creator 4.3 and PDL 3.1.2
Thanks
Show LessHi,
想咨询一下,想使用PSoC Creator进行PSoC 62 512K和PSoC 62 2M芯片开发,发现在device selector里没有对应的型号(TQFP封装或QFN封装)如图,请问是需要额外的补丁或是使用ModusboxTool进行开发么?ModusboxTool里如何选择芯片型号而不是选择BSP?
Best Regards
Simon
Show LessIn the schematic for the CY8CMOD-062-4343W (https://www.cypress.com/file/457816/download page 4), I see the part number for the PSOC6 is listed as:
CY8C624ABZI-S2D44
When I look for this part in the "Device Selector" in PSOC creator, I don't find this part number. What is the exact part number for this?
Show LessHi,
I am using PSOC6 Wi-Fi BT kit with PSOC creator. I tried loading one of the example related to TFT display. In the schematics the components are not getting loaded. What should I be doing to fix this?
Hi all,
I'm using CYBLE-416045-02 mcu and in my application I'm displaying output in ili9341 320x240 lcd using Spi. But due to other tasks data transfer speed is not enough.
Hence we decided to use Dma peripheral to flush the data into to lcd through spi. But I dont know how should I manage the cmd/data pin of the lcd as this pin needs to be clear for sending command byte and set when sending data bytes. So my question is how to solve this problem and please provide me an sample project if you have where lcd is getting driven using Dma through spi.
Thankyou
Show Less