PSoC™ 6 Forum Discussions
Hi Community,
I want to port CYW20706 A2DP_Sink program to CY8CKIT-062S2-43012.
Hello,
I'm working on the PSoC6 BLE Pioneer Kit CY8CKIT-062-BLE in modus toolbox and having trouble sending and receiving inputs from the keyboard. Id like to be able to type in the terminal and have it show up after hitting enter.
I have retargetIO initialized and printf working but it gets/getchar/fgets aren't loading anything to the terminal. Could my issue be the terminal I'm using is the "open a terminal" button on the modus toolbox banner? Or is there something else I'm missing.
Thanks,
Ryan
Show LessHi Community,
I am using CY8CKIT-062S2-43012 kit. I want to run HFP (Hand Free Profile) and A2DP (Advanced Audio Distribution Profile). I am not getting these two profiles in Eclipse IDE ModusToolbox 2.4.
Show LessHi,
there is a way to get the unix time ( Seconds since January 1, 1970 ) from RTC?
I have tried with mktime() but it doesn't work.
Thanks,
Giuseppe
Show LessHi!
I'm trying to use the backup registers (BREG) on PSOC6/CY8CPROTO-062-4343W to set a value before rebooting.
Documentation on this topic is either elusive, or light.
I started here in section 3.3.5 - https://www.cypress.com/file/385936/download
I found a declaration of a struct BACKUP_V1_Type, which contains 64 bytes of BREG in cyip_backup.h.
There's no detail how to use it tho. Doesn't look like it contains register addresses at all, and just a data structure.
I found a register address for BREG on another PSOC platform in a technical reference manual, but it is not retaining any information when I use CY_SET_REG32 and CY_GET_REG32. Can someone point me to the information? Maybe the TRM for the platform I'm using?
Thanks!
Show LessHi everyone. I have the following issue. I just installed the new version of IDE Modus Toolbox in 2.4.
After going through the entire installation procedure on my Linux Manjaro machine.
My sample applications compile fine, but when I do Debug or Program it throws the following error and does not allow me to program my PSoC6.
Could not determine GDB version after sending: /home/user/ModusToolbox/tools_2.4/gcc/bin/arm-none-eabi-gdb --version, response:
I want to emphasize that I had previously installed the Modus Toolbox 2.3 version and it was working fine
Can you guide me to solve this problem, please?
Show Less
Found 28 .mtb file(s)
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/deps/TARGET_CY8CKIT-062S2-43012.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/deps/anycloud-ota.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/libs/abstraction-rtos.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/libs/aws-iot-device-sdk-embedded-C.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/libs/aws-iot-device-sdk-port.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/libs/bluetooth-freertos.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/libs/btstack.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/libs/capsense.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/libs/clib-support.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/libs/connectivity-utilities.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/libs/core-lib.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/libs/core-make.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/libs/freertos.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/libs/http-client.mtb"
Processing file "D:/Neelakanta/modusws6/AnyCloud_OTA_Using_HTTPS/libs/lwip.mtb"
fatal: unable to access 'https://git.savannah.nongnu.org/git/lwip/': SSL certificate problem: certificate has expired
ERROR: Unable to checkout "lwip". This is not a valid git repository.
==============================================================================
ERROR: --ABORTING--
: Script : C:/Users/Pro/ModusToolbox/tools_2.3/make/getlibs.bash
: Bash path : /usr/bin/bash
: Bash version: 4.4.12(3)-release
: Exit code : 1
: Call stack : trap_exit error perform_git process_mtb extract_data find_mtbs main
fatal: unable to access 'https://git.savannah.nongnu.org/git/lwip/': SSL certificate problem: certificate has expired
make: *** [C:/Users/Pro/ModusToolbox/tools_2.3/make/getlibs.mk:126: getlibs] Error 1
Project "AnyCloud_OTA_Using_HTTPS" failed to create.
"make getlibs" failed.
Failed to create and export "AnyCloud_OTA_Using_HTTPS" application.
Show Less
Hi,
I am working with a PSOC6 device built into a PCB, and it turns out the Tx and Rx pins need to be the other way around. Is there ANY way to do this through PSOC Creator WITHOUT needing to perform tiny surgery on my circuit board? The UART is primarily meant to be a dev interface so simple reading and writing, I just want to know if this is possible.
To be a little more specific, I need to change P10.1 to P10.0 and vice versa, but the Pins menu doesn't allow that it seems.
Thank you!
Show LessHi,
I've successfully have gotten my CY8CPROTO-062-4343W board configured as MSC device to work. I'm using the MTB project "USB_Mass_Storage_File_System".
However, every time I record another sound file (rec_xxxx.raw), the PC host doesn't see it unless I either unplug the USB connection or perform a board RESET.
Is there a event signal I can send to the PC host to request a refresh of the cached directory info the PC host has?
I realize that, in general, it is assumed with the MSC device, the host has 100% control of the storage device. It is not normally expected for the MSC device to "self-update" its contents.
Maybe there is an event packet to send the PC host to check if the directory has been corrupted?
Show LessHello everyone,
I'm currently working on a project for my PSoC 6-based Cypress board, and I need a simple and quick way to set up my board as a HTTP client to download data (in a JSON format) from a server.
Are there any libraries or APIs from Cypress that implement RESTful services ?
Show Less