Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

gkuhn100
PSoC™ 6
Hello, Whenever I attempt to build a sample Application in Modus Toolbox using the PSoc6 I get the following two errors displayed in my terminal. Anyo... Show More
SaGa_4641021
PSoC™ 6
Hi PSoC63 datasheet (specifically CYBLE-416045-02) states "1.71 V to 3.6 V Operation". Can I power the PSoC directly from LiPO battery without using a... Show More
mingguy
PSoC™ 6
Hi, I am trying to use some radar ifx libraries that require math.h functions such as hypotf and sqrtf. However the compiler cannot find where these f... Show More
Dumko
PSoC™ 6
Hello. I have MiniProg3 and am using PSoC Programmer 3.29.5. I have a project not in PSoC Creator. When i try to upload hex to PSoC Programmer - i h... Show More
Atsumin7110
PSoC™ 6
I'm making an application on the microcontroller with CYBLE-416045-02. However, it suddenly stops working after 10 or more minutes passed. I doubt tha... Show More
GrCa_1363456
PSoC™ 6
What is the correct minimum endurance for embedded flash in a PSoC 6? Datasheets for PSoC 6 claim 100k cycles minimum for Flash Endurance. TRMs claim ... Show More
Jonny-Fission
PSoC™ 6
Our company has a device that uses two microprocessors; the CY8C4245PVI-482 and the CYBLE-416045-02 (PSoC 4 and PSoC6).  The device will be in a case ... Show More
prk_4086136
PSoC™ 6
Hello, I made a custom BSP for my part CY8C6347FMI-BLD33, and started a new dual core application using the example. I am able to successfully compile... Show More
HotPins
PSoC™ 6
Dear Sir or Madam, I have some underlying logic questions I'd like to ask about Capsense. 1. I don't have ADC set in the setup, but Capsense is still ... Show More
YongseokJeon
PSoC™ 6
Hi, I'm using CY8CKIT-062-WIFI-BT EVK. I'm creating a PWM waveform with P0.3 using TCPWM[0].CNT[1]. Is there a way to use another Timer (e.g. TCPWM[0]... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.