Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 6

Recent discussions

Sort by:
alexpark
PSoC™ 6
Hi All, In the case of the CYB06445LQI-S3D42 product, is there any data that shows how many ms it takes to 'Secure Boot' from the device reset to the ... Show More
NiBu_4687336
PSoC™ 6
Hi. I'm trying to use the HAL System Power Management library to put the CM4 to sleep. So far, I've had no luck, and as I have found too many times, t... Show More
Len_CONSULTRON
PSoC™ 6
I'm using a a CY8CKIT-062-BLE with the EINK display. I have two projects using this kit. One works to update the display the other does not. On the on... Show More
Oliver_Choe
PSoC™ 6
Hi  I made custom BSP for CY8C6244AZI-S4D93. I was trying to add DAC configuration using MTB but I think there are some problem with connection verifi... Show More
shlim
PSoC™ 6
PSoC 6 MCU: CY8C62x6,CY8C62x7 Datasheet I think that it was printed incorrectly in Address Map. Page 12 of 77 0xE010 0A000 – 0xFFFF FFFF Device Device... Show More
YSJE_3566666
PSoC™ 6
Hello, I have questions about Flash and Emulated EEPROM. 1. The flash endurance is described in the datasheet as 100k cycles.Does each row of flash in... Show More
Tim_Shih
PSoC™ 6
Dear Receiver,  I practice "PSoC™ 6 MCU: MCUboot-based basic bootloader" by using the example code in the following GitHub link... https://github.com/Infineon/mtb-example-psoc6-mcuboot-basic... Show More
inja_4756821
PSoC™ 6
Dear Expert. Hello. I have a question as below. I'm trying to use the emwin Driver provided in PSOC6. (pre included Driver at MTB IDE) 1. Is there a e... Show More
YSJE_3566666
PSoC™ 6
Hello,I'm trying to program a hex file to CY8C6136 using Segger J-flash (V7.66a). Q1. Which one should I choose from the list below in the Target Devi... Show More
stratuscent_mtl
PSoC™ 6
Hi, We are trying to port the existing firmware in PSOC Creator to ModusToolbox to make it available for the new chips. However, the biggest challenge... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.
Top labels