Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 6 Forum Discussions

Recent discussions

Sort by:
ScKi_1600301
PSoC™ 6
I have a simple program for reading the JEDEC information from a serial flash chip using the low-level API.static void SPI_FlashWriteByte(uint8_t byte... Show More
PrMa_4715901
PSoC™ 6
Recently I was working on a project to display multiple bitmaps on the TFT screen of CY8CKIT-062-WiFi-BT. But soon I realized that the converted image... Show More
StLe_4753786
PSoC™ 6
Hi,Could anyone point me to an example showing PSoC6 with internet connectivity using a GSM modem on an UART port (e.g. SIMCom or Quectel modem)?  I a... Show More
AlSt_3233956
PSoC™ 6
Hello,using PSoC Creator 4.3 with PDL v3 = 3.1.2 and PDL v2 = 2.1.0. The BLE Device is configured as Peripheral the connection settings are the follow... Show More
ChRe_4711096
PSoC™ 6
The attached project contains ofthe SAR ADC with one analog MUX for each inputan 8-bit datapath with parallel out that selects the analog MUX inputsa ... Show More
ChRe_4711096
PSoC™ 6
I'm looking for ways to ease the chip from some combinatorial logic. I have 4 instances of a component that has a 4-input OR gate, and I'm tempted to ... Show More
NiLe_4630071
PSoC™ 6
The BLE event handler that I set up with CyBLE_Start gets called with event = 0x00010005 twice after CY_BLE_EVT_GAP_ENCRYPT_CHANGE when accessing the ... Show More
GuGa_1322886
PSoC™ 6
I'm working with Mbed Studio 6.1 and CY8CPROTO-062-4343W on a project with MBed OS 6.2Following the sample code of the HAL documentation I created the... Show More
WiWi_4702256
PSoC™ 6
I need to be absolutely certain of the following: My hardware engineer asked me to verify:P10_0 can be configured A to DP11_2 thru P11_6 can be config... Show More
BiMa_2659891
PSoC™ 6
HI Cypress Team,In my custom board which uses PSOC62 BGA part: CY8C624ABZI-S2D44, we are facing issue in configuring the pull-down.Can you please let ... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.