Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 6 Forum Discussions

BloedeBleidd
PSoC™ 6
TLS example
solved msg Solved
Hello, Is there an example of an application that allows TLS authentication (just authentication, without any further information exchange) via UART, ... Show More
jayesh_joshi
PSoC™ 6
In my CY8CKIT-062S2-43012 board I looking for expanding RAM for operations of mallocs functions. I have come across one example (QSPI_F-RAM_Access) wh... Show More
remusmp
PSoC™ 6
Hello everyone, I made a testing firmware that blinks an LED, which runs fine on my development board CY8CKIT-062S2-43012 but not on my custom board, ... Show More
micro-atama
PSoC™ 6
Hello, when I add svd file to see the peripheral register,every port (port0 to port14) has the same address. ※modus version is 2.2 But in another vers... Show More
Demi1
PSoC™ 6
Modus ToolBox
solved msg Solved
Hello, I am a novice, just contacted Modus ToolBox software, using the kit is CY8CKIT-062S2-43012; now I want to create a new project to practice, but... Show More
Akash-USC
PSoC™ 6
Hi All,   Can someone give me an estimate of the power consumption of the chipset in the following modes. 1. Deep Sleep 2. ADC Data Input 3. Data Proc... Show More
GrCa_1363456
PSoC™ 6
What are the minimum requirements that an MCU must have to support the SDIO interface of a hosted WiFi/BLE module? For example, how can I tell if a CY... Show More
ravo
PSoC™ 6
Dears, I am unable to find "Tool Settings" under C/C++ Build as shown in some tutorials, manuals for Modus Toolbox IDE. Where are these settings in Mo... Show More
lussmar
PSoC™ 6
Hello! Im currently trying to read a JSON file in my psoc project for the cyproto-063-BLE but i cannot get it to work.  I have a JSON file that im try... Show More
Akash-USC
PSoC™ 6
Hi All,   Could any of you help me in setting the sampling frequency of the PSOC6 chipset ADC to 2KHz? The minimum clock frequency the ADC can take in... Show More
Forum Information
PSoC™ 6

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.