PSoC™ 6 Forum Discussions
I am trying to program CYBLE-416045-02 using Flasher ARM in Stand-alone mode. It turns the red led on, when I press the [PROG] button. Here, the use cable from the flasher is connected to a power source but not a PC.
Flahser log shows:
ERROR: Failed to download RAMCode.
SN: 0 - Failed
I could successfully program the target device using J-Flash software. Flahser project set up is as follows:
Does anyone have some clue on this issue?
Thank you!
Best regards,
Show LessHello,
Does the CY8C6136FDI-F42's flash have ECC (Error Correction Code)?
I'm trying to detect if there is an error when writing and reading data to flash.
I wonder if there is something like ECC on the STM32L412RB.
I attach the relevant content.
Best Regards,
YS
Hi Community,
I want to do bootloading using USB in Psoc 6(CY8C6247BZI-D54). For that I tried USB in empty project and I found Error.
That Error is:
Invalid connection for clock "USBFS_devClk" connected to "\USBFS:USBFS\:clk_usb_dev". The component input does not support generated clocks.
I tried so many things and it is still not working.
Can somebody help me to solve this Error? Can someone send the link for code example of USB in PSOC Creator for PSOC6?
Thank You,
Anjali
Show Less
Hello,
We will be interfacing this Micron Flash Part MT29F2G01 with a PSoC 62(CY8C6247FDI-D32) over QSPI. Are there any drivers/examples that I can use to expedite my work? I see that the Modus Toolbox has an QSPI example for the CY8CKIT-062-WiFi-BT devkit which uses a NOR Flash; but the Micron par I referred to above is a NAND flash. Is that the best starting code I should use or is there anything better? Thanks.
Show LessHi,
I want to interface a QSPI NOR Flash (W25Q16JV ) in PSoC6 MCU using PSoC Creator IDE. Is there any configurator available as in Modus toolbox for PSoC Creator?
I have gone through the example code for SMIF interface using the WiFi-BT pioneer KIT.
Please help.
regards,
Vinu
Show LessHi - I'm trying to start a new PSoC Creator project for a PSoC 6 device. It is not listed in the Device Selector. I'm trying to use this PSoC 6: cy8c6144lqi-s4f82
Why is it missing in the device selector lists? I updated the tool, no change.
Show LessHi,
My device uses "Just Works" pairing and bonding. The issue I get is when the device is unpaired/forgotten by the phone. When trying to pair the phone and the device again, pairing seems to work, but they can't seem to communicate together as if no new keys were exchanged. For it to work, I need to erase the phone from the bonded device list on the device as well.
Is this expected behavior or is it something that could be fixed in my application?
Show LessHas anyone had any success using Cy_BLE_GetWhiteList(), or know of an example?
Every permutation of input parameter I try results in a CY_BLE_ERROR_INVALID_OPERATION response. Any guidance would be appreciated.
Show Less
On CY8C6347BZI-BLD54 i am trying to internally connect RX_SCK with TX_SCK and RX_WS with TX_WS. like showed in the two images below. Psoc creator complains about it. is there a walkaround? maybe using DSI?
Smart IO is not an option since its not available on Port 5 ( where the I2S subsystem is harwired)
thanks!
Show LessHi,
I am trying to use Em_EEPROM to store some non-volatile information in the firmware.
What I want to do is edit the data in the corresponding address of the .HEX file, and program the file into PSoC, then read the data using the firmware.
I am meeting the following questions:
1. How to edit the HEX file? I think there is checksum part in the HEX file, so directly editing the file will cause the error during programming.
2. What is the address that corresponds to the logical address 0 of the em_eeprom? I found the following code in "dfu_cm4.ld", so is the address "0x14000 0000" is the logical address 0 of the em_eeprom?
Really hope someone can kindly help me out!
Best regards
Show Less