PSoC™ 6 Forum Discussions
text.format{('custom.tabs.no.results')}
Hi Community,
Can We use USB_CDC in Device Firmware Update for PSoC 6(CY8C6247BZI-D54) in PSoC Creator?
If it is possible then somebody please share the code example for that!
Thank You,
Anjali
Show LessHi
Can we use fTDI USB UART TTL for programming PSOC6 MCUs.
Hello,
I am using a PSOC 6 prototyping board and I am trying to display 3 voltages that are labelled (ref,Temp_sens,battery_level). Can you please check if my project is correct?
Thank you
Show LessHello,
I am using a PSOC 6 prototyping board and I would like to have a code that lets me control the drive state mode ( high, low) in the actual software? what code can I use for that?
Thank you
Show LessHi,
We have been using self-capacitance (CSD) to measure proximity. However, we have observed that the raw count drifts despite the lack of environmental change. Our experimental environment was held at constant temperature and humidity. There was also no movement of any objects over the window of the experiment (5 mins). We tried using both a button widget and a proximity widget for the measurement but we have repeatedly observed a 100-200 drift of the raw count. Are there any settings that could be changed to mitigate this situation?
Thank you for your help!
Show LessHI
What is the output voltage and output current of the dac 12 bit in psoc6 (CY8C6137BZI-F34)
thanks
Hello,
I am trying to do the following application :PSoC 6 MCU with BLE Connectivity: RTC with Current Time Service (RTOS) (infineon.com). But I am using an OLED display. I want to display the time on the screen and be able to connect it to a phone through Bluetooth. I have attached the project. Can anyone help?
Thank you,
Ali Issa
Show LessHi,
I create a project, using CY8C61137BZI.
I'm using all the IOs that the device has.
I did only the drawing to allcate all the pins.
When I build the project, I'm getting errors regarding few output pins.
I attached the project.
BR
Shmuel
Show LessThis is for Windows 10, Modustoolbox (latest) and CY8C624AAZI-S2D44 (these were early, 4 yrs old, engineering samples. COVID delayed everything)
I managed to create a custom BSP for my board (using latest modustoolbox) and now I'm trying to program some functions to check the board. Other than a warning about kitprog3 needed to be updated it programs without errors. I have a couple of debug LEDs connected (P8.2 and P8.3). LEDs turn on when a ground (low) is present at those pins. I can't get that done. I'm using the Empty PSoC 6 app to create a project from my BSP (Import BSP). I was trying to use code to output a low on the LEDs pins but I'm so new at PSOCs that I decided to just leave the For(;;) in the main function empty and try to set the pins in the device configurator to low for the LEDs and High on some others to see if that's working. Nope, nothing works. It looks like the pins are floating. The drives for outputs is set to "strong drive, input buffer off". I've changed the oscillator from a crystal (P12.6 and P12.7) to the internal osc. but still nothing. I tried to output the internal clock to "external pin" and I see nothing on P0.5.
I read here that the first thing at start time is "Executes any hardware-specific initialization code". Is this the device configurator settings?
I do have the WCO enabled and connected. I saw a message in the device configurator that this will delay startup until ...something. What if there is something wrong with my hardware and the WCO never starts? will this prevent the startup sequence from executing?
Any help is appreciated. Thanks.
Show Less