Recent discussions
Hello,
I am trying to generate an output frequency of 6 MHz using a PSOC 6 prototyping board but every time I measure the pin using an oscilloscope its not giving me the required frequency. I have attached the project. Can anyone help please?
Thank you
Show Less
I can't find “Disassembly Window” here.
From the Debug menu, choose Windows > Disassembly.
Hi,
I am using CYBLE-343072-02 module as mesh node and PSoC™ 6 Wi-Fi BT Prototyping Kit as a gate way. Mesh part got completed successfully but I cannot able to configure the PSoC™ board with MESH board through Bluetooth and i need to send data to server through WIFI .How we can integrate that?. What are the steps we need to take for that.
Show Less
Hi,
I'm using the PSoC creator 4.2 version to design the device CY8C6137BZI-F54 .
I have few iput discretes and few output discretes.
When I used PSoC5LP component I used status register and control register for that.
What to use for PSoC6?
BR
Shmuel
Show LessThe installation instructions of the ModusToolbox say that if you have a custom path you need to edit the environmental variables location from the environmental dialog.
How do I find the Environment Variables dialog? I've looked at all the dropdowns such as File, Edit, Navigate, etc...
I've gone through all the properties of each item I can right click on.
Thanks
Show Less
Hello,
I am trying to generate a frequency of 6 MHz using a Psoc 6 prototyping bord. Can you please check the attached project if this is correct?
Thank you
Show LessWhere is there more description of the Alternate Functions in PSoC 6 devices?
A description of Table 8 and the acronyms used such as ACT would be helpful. Reference Table 8. Multiple Alternate Functions of the "PSoC 6 MCU: CY8C62x6 CY8C62x7 Datasheet" Rev *N
The "Pinouts" section on Page 22 of the "PSoC 6 MCU: CY8C62x6 CY8C62x7 Datasheet" Rev *N proports to provide a link to "datasheet web page" for more information on Alternate functions. The link under "datasheet web page" provides a circular reference back to the same "PSoC 6 MCU: CY8C62x6 CY8C62x7 Datasheet".
"Note: The CY8C62x6/CY8C62x7 datasheet web page contains a spreadsheet with a consolidated list of pinouts and pin alternate functions with HSIOM mapping."
I have not yet been successful in my search for any explaination of "Alternate Functions" in the Technical Reference Manuals or Device Configurator Guide. I suspect there may be some explanation in the Peripheral Driver Library (PDL) documentation. Unfortunately, the search tool in the PDL documentation is only useful if you know the exact spelling of a command or parameter being searched.
There are some hints in the Community. I suspect there's an explanation somewhere.
- PSoc 63 SDA SCL @ https://community.infineon.com/t5/PSoC-6/PSoc-63-SDA-SCL/m-p/330353#M11544 discusses how to use some of the information in Table 8 - apparently through the use of PSoC Creator or Device Configurator.
- Switching between UART and MUX functionality on the same pins - KBA233908 @ https://community.infineon.com/t5/Knowledge-Base-Articles/Switching-between-UART-and-MUX-functionality-on-the-same-pins-KBA233908/ta-p/327395 discusses the use of Alternate functions without providing the rules. This is a nice example although it's using PSoC Creator instead of ModusToolbox.
Greg
Show LessHi.
I'm using CY8C6137BZI-F54 at my design.
I have 15 analog inputs that are connected to port 9,10.
When I put the pin assignment all the analogs at port 9, there is a worning about routing congestion.
What do I need to do?
BR
Shmuel
Show LessHi,
I am using ssd1306 0.96 inch OLED screen and I am using it for PSOC 6- PSOC63 (CY9CKIT-062-BLE). Which pins other than P9[0] to P9[4] I can use as I am already using them?
Show LessThe psoc6ble program cannot execute After migration
1 The ori PSOC6 BLE program named "CE217639_BLE"Heart_Rate_Client01" was created frome creater software,The program is uesd for poc6ble KIT,
2 The MUC I use is CY8C6347LQI-BLD52 which different from the ori Porgam used,so the ori program is miagrated to a new one;
3 but the new program that only MUC version was changed could not work at all,could not debug either
4 The miagrated program and schematic diagram contained in the attachment
5 MY PCB has 2 floors
/**********************************/
1 原程序是 creater 软件上的 CE217639_BLE"Heart_Rate_Client01,这个程序是用于开发板上的
2 我自己的MCU 型号是 Y8C6347LQI-BLD52,所以需要在原程序更改 MCU型号
3 在原有程序知识 MCU 型号更改了,在新板子上无法启动 ,无法进入debug
4 附件有移植后的程序和我的PCB 原理图
5 我的PCB 是2层