Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

BUTA_1301626
Level 4
Level 4
50 replies posted 25 replies posted 10 replies posted

I have RF Project. RF receiver will be 100m distance between RF transmitter. Which communication block is better to use? Would you help me decide the communication block?

3 Replies
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

Please povide transceiver type/model that is going to be used for communication.

0 Likes

The properties of the receiver and the transmitter to be used are as follows.

UTR-C12U UHF FSK transceiver module, Basic Standards of Short Distance Access Radio Devices Regulation on the Principles of Installation and Use (TGM-STK-001) 433-434MHz. Designed to cover the ISM band related part. UTR-C12U is designed for PCB assembly. An antenna can be connected using a simple cable.

Ekran Alıntısı2.JPGEkran Alıntısı.JPG

0 Likes

It seems like the UTR-C12U uses UART to communicate with CPU/PSoC. Can you kindly attach the english version of the datasheet, so we can confirm.

Best regards,

Sampath