cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 6

BUTA_1301626
New Contributor II

I have RF Project. RF receiver will be 100m distance between RF transmitter. Which communication block is better to use? Would you help me decide the communication block?

0 Likes
3 Replies
odissey1
Honored Contributor II

Please povide transceiver type/model that is going to be used for communication.

0 Likes
BUTA_1301626
New Contributor II

The properties of the receiver and the transmitter to be used are as follows.

UTR-C12U UHF FSK transceiver module, Basic Standards of Short Distance Access Radio Devices Regulation on the Principles of Installation and Use (TGM-STK-001) 433-434MHz. Designed to cover the ISM band related part. UTR-C12U is designed for PCB assembly. An antenna can be connected using a simple cable.

Ekran Alıntısı2.JPGEkran Alıntısı.JPG

0 Likes
SampathS_11
Moderator
Moderator

It seems like the UTR-C12U uses UART to communicate with CPU/PSoC. Can you kindly attach the english version of the datasheet, so we can confirm.

Best regards,

Sampath

Top labels