Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Anyone know the USB pin numbers for the 116-BGA?  Can't seem to find them in the datasheet.  the "Hardware Design Considerations" document references pins on port 14 but there is no port 14 on the 116-BGA package. 

0 Likes
1 Solution
RodolfoGL
Employee
Employee
250 solutions authored 250 sign-ins 5 comments on KBA

Hi,

We are still working on providing the USB functionality for PSoC 6. At the moment, we don't have any 116-BGA part that will support USB. The only packages available are 80-WLCSP and 124-BGA.

Regards,

Rodolfo Lossio

View solution in original post

8 Replies
RodolfoGL
Employee
Employee
250 solutions authored 250 sign-ins 5 comments on KBA

Hi,

We are still working on providing the USB functionality for PSoC 6. At the moment, we don't have any 116-BGA part that will support USB. The only packages available are 80-WLCSP and 124-BGA.

Regards,

Rodolfo Lossio

Any ETA for this part?

0 Likes

rlos​ you mentioned that USB exists on the CSP and 124-pin BGA parts.   

please direct us to the correct part-no for these, I can't find it in the datasheet, only

     BZ = 116-BGA

     FM = 104 MCSP

Spec ID

Package

Description

Package Drawing Number

PKG_2

104-MCSP

104-MCSP, 3.8 5 0.65 mm height with 0.35-mm pitch

002-16508

PKG_4

116-BGA

116-BGA, 5.2 6.4 0.5 mm height with 0.5-mm pitch

002-16574

0 Likes

You can find the datasheet here:

http://www.cypress.com/file/385916/download

0 Likes

Sorry, forgot to mention we need family = 3 == Connectivity,

i.e.

   BL = PSoC 6A-BLE

0 Likes

At the moment, there is no part supporting BLE and USB at the same time.

0 Likes

ok. will this happen within Q1 2018?

0 Likes

I don't know. Which company you work for? And what kind of application you are building?

0 Likes