Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
JCD
Level 3
Level 3
50 sign-ins 25 sign-ins 10 replies posted

Originally, there was no problem. Suddenly, the code could not be downloaded. The following is info:

 

Started by GNU MCU Eclipse
Open On-Chip Debugger 0.10.0+dev-4.1.0.1058 (2020-08-11-03:47)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "swd". To override use 'transport select <transport>'.
adapter speed: 2000 kHz
adapter srst delay: 25
adapter srst pulse_width: 25
** Auto-acquire enabled, use "set ENABLE_ACQUIRE 0" to disable
cortex_m reset_config sysresetreq
Warn : SFlash programming allowed for regions: USER, TOC, KEY
Info : CMSIS-DAP: SWD Supported
Info : CMSIS-DAP: FW Version = 2.0.0
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : SWCLK/TCK = 1 SWDIO/TMS = 1 TDI = 1 TDO = 1 nTRST = 0 nRESET = 1
Info : CMSIS-DAP: Interface ready
Info : KitProg3: FW version: 2.21.1005
Info : KitProg3: Pipelined transfers enabled
Info : VTarget = 3.328 V
Info : kitprog3: acquiring the device...
Error: kitprog3: failed to acquire the device
Info : clock speed 2000 kHz
Error: DAP 'psoc6.cpu' initialization failed (check connection, power, etc.)
Info : psoc6.dap: powering down debug domain...
Warn : Failed to power down Debug Domains

0 Likes
2 Replies
Rakshith
Moderator
Moderator
Moderator
250 likes received 1000 replies posted 750 replies posted

Hi @JCD

Can you please let us know if you are using a Cypress Kit or a custom board? If it is a custom board, can you please share the power and XRES schematics and let us know the programming parameters. If it is a Cypress Kit, which kit are you using?

Additionally, please let us know the programmer (KitProg3 or MiniProg4) and the version of ModusToolbox used.

Thanks and Regards,
Rakshith M B
0 Likes
Rakshith
Moderator
Moderator
Moderator
250 likes received 1000 replies posted 750 replies posted

Hi @JCD

Thread was locked due to inactivity for long time, you can continue the discussion on the topic by opening a new thread with reference to the locked one. The continuous discussion in an inactive thread may mostly be unattended by community users.

Thanks and Regards,
Rakshith M B
0 Likes