Is there an application note that explains the complexity of the interacting between the CM4 and CM0+ using the IPC channels and couples that with understanding Flash write requests for RWW and non-RWW options?
Solved! Go to Solution.
There are no application notes specifically on writing PSoC 6 flash. However, there are app notes on bootloading (AN213924) and on IPC usage (AN215656).
In addition, there are multiple code examples regarding IPC and flash. In PSoC Creator, click Find Code Example and look for "IPC" or "CE216795". For flash writes, look for "flash"; you will find multiple flash write and bootloader code examples.
You can also find details on how flash writes are implemented in a PSoC 6 technical reference manual (TRM); see the chapter on nonvolatile memory programming.