Hi,
Currently I am testing aws_demos example in ModusToolbox2.2.
When I was using CY8CPROTO-062-4343W Rev06(IC marked with A33), I am able to reprogram and switch between different projects.
But when I changed to CY8CPROTO-062-4343W Rev08(IC marked with B33), I only programmed once and it seems the program had not been properly flashed into the board. The debug port was totally shut down and I cannot reprogram any more.
Even when I pressed SW3 to switch mode, also can not do it. It will go back to "KitProg3 CMSIS-DAP" in device manager. Please refer to the attached picture. I already killed several Rev08 boards when I was trying to program aws_demos into these Rev08 Boards.
Below is the log from Cypress Programmer when I'm trying to connect.
Please help to analyze and debug. Thank you very much.
Solved! Go to Solution.
Hello,
There was bug in the older version of Cypress' amazon-freertos 201910-MTBAFR1951 causing the issue you observed.
Please check this thread for details.
Cheers!
It looks the KP3 could be recognized on your end, but the device could not, right?
It always shows failure log when you click the "Connect" button of Cypress Programmer?
It's fine for all Rev06 boards, but not for all Rev08 boards?
It looks the KP3 could be recognized on your end, but the device could not, right?
Yes, "KitProg3 CMSIS-DAP" still can be seen in device manager
It always shows failure log when you click the "Connect" button of Cypress Programmer?
Yes, and also can not program in ModusToolbox
It's fine for all Rev06 boards, but not for all Rev08 boards?
Yes, it is fine for Rev06 boards, but can not reprogram for all Rev08 boards.
Below is the log from ModusToolbox when using Rev08.
Hi
Could you kindly help to take a look at this issue? It is quite urgent and serious for us. Thank you very much.
you need to use DAPLINK mode to program.
Hello,
There was bug in the older version of Cypress' amazon-freertos 201910-MTBAFR1951 causing the issue you observed.
Please check this thread for details.
Cheers!