- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am working on IOT app and I am un able to create project using project creator.
Also I go through this conversation but did not find where I have to type that command.
Bellow are which I get when I create project using project creator.
Submodule path 'libraries/standard/corePKCS11/source/dependency/3rdparty/pkcs11': checked out '9304ef6842d08d881ccd1daa8d3a428f3a9671ee'
Processing file "D:/Project_2/AWS_App/AWS_IoT_OTA_Using_MQTT_2/libs/aws-iot-device-sdk-port.mtb"
Processing file "D:/Project_2/AWS_App/AWS_IoT_OTA_Using_MQTT_2/libs/bluetooth-freertos.mtb"
Processing file "D:/Project_2/AWS_App/AWS_IoT_OTA_Using_MQTT_2/libs/btstack.mtb"
Processing file "D:/Project_2/AWS_App/AWS_IoT_OTA_Using_MQTT_2/libs/capsense.mtb"
Processing file "D:/Project_2/AWS_App/AWS_IoT_OTA_Using_MQTT_2/libs/clib-support.mtb"
Processing file "D:/Project_2/AWS_App/AWS_IoT_OTA_Using_MQTT_2/libs/connectivity-utilities.mtb"
Processing file "D:/Project_2/AWS_App/AWS_IoT_OTA_Using_MQTT_2/libs/core-lib.mtb"
Processing file "D:/Project_2/AWS_App/AWS_IoT_OTA_Using_MQTT_2/libs/core-make.mtb"
Processing file "D:/Project_2/AWS_App/AWS_IoT_OTA_Using_MQTT_2/libs/cy-mbedtls-acceleration.mtb"
Processing file "D:/Project_2/AWS_App/AWS_IoT_OTA_Using_MQTT_2/libs/freertos.mtb"
Processing file "D:/Project_2/AWS_App/AWS_IoT_OTA_Using_MQTT_2/libs/http-client.mtb"
Processing file "D:/Project_2/AWS_App/AWS_IoT_OTA_Using_MQTT_2/libs/lwip.mtb"
fatal: remote-curl: fetch attempted without a local repo
ERROR: Unable to checkout "lwip". This is not a valid git repository.
==============================================================================
ERROR: --ABORTING--
: Script : C:/Users/Lenovo/ModusToolbox/tools_2.4/make/getlibs.bash
: Bash path : /usr/bin/bash
: Bash version: 4.4.12(3)-release
: Exit code : 1
: Call stack : trap_exit error perform_git process_mtb extract_data find_mtbs main
fatal: repository '/cygdrive/c/Users/Lenovo/.modustoolbox/cache/git/https___git.savannah.nongnu.org_git_lwip/lwip' does not exist
make: *** [C:/Users/Lenovo/ModusToolbox/tools_2.4/make/getlibs.mk:121: getlibs] Error 1
Project "AWS_IoT_OTA_Using_MQTT_2" failed to create.
Failed to create "AWS_IoT_OTA_Using_MQTT_2" application.
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
Hi @Sachin_Patel ,
Can you please try and locate the .modustoolbox path "/cygdrive/c/Users/Lenovo/.modustoolbox/"
In my PC I have it in the path "C:\Users\<userName>\.modustoolbox"
You will find a folder named cache in the same.
Can you delete this cache folder and try to create the project once again in ModusToolbox.
Warm Regards
Alen
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
Hi @Sachin_Patel ,
Glad the issue is resolved.
Ill make a note of this issue and pass on the same to my internal team to see if we can figure out the cause of the same. Thank you for pointing it out.
Warm Regards
Alen