Hello,
I use PSoC Creator generates a CMSIS-Pack(PSoC61(CY8C6137BZI-F14)),and install it.
When open keil Project,below message is appear->
Error loading software packs
Cypress.Pack.1.0.0: device 'CY8C6137BZI-F14_P61': error #531: ResetProcessor property uses undefined processor 'CortexM0p'
Cypress.Pack.1.0.0: device 'CY8C6137BZI-F14_P61': error #531: debug property uses undefined processor 'CortexM0p'
Why did this error occur?Can you help me solve it?
even though use this error pack,keil project can build OK
Whether this error will have an impact when it is used?please help me
the problem arrange in attachment ,please refer it
消息编辑者为:wang xue
Solved! Go to Solution.
Hello Ryanz,
thanks very much!
I create uVision Project step by step,but this warning still appeared,
I modify the pdsc file(C:\Keil_v5\ARM\PACK\Cypress\test\1.0.0\Cypress.test.pdsc)this warning is disappeared.
Please read details in "Creating µVision Projects for PSoC 6" in help file of PSoC Creator. And follow its rules step by step.
Thanks,
Ryan
Hello Ryanz,
thanks very much!
I create uVision Project step by step,but this warning still appeared,
I modify the pdsc file(C:\Keil_v5\ARM\PACK\Cypress\test\1.0.0\Cypress.test.pdsc)this warning is disappeared.