Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hello,

I think that NVIC of M0+ can select 32 interrupts from 147 as for block diagram of TRM.

But we cannot set interrupt number of except of 3 to 29.

Why cannot we chose the number such as 1, 2, 30 or 31?

Best regards,

1 Solution
MeenakshiR_71
Employee
Employee
100 likes received 50 likes received 25 likes received

Hello,

Yes M0+ allows 32 interrupts as captured in TRM. However, CM0+ interrupt channels 0-2 and 30-31 are reserved for system use, inter-processor communication, and the crypto driver. Other IRQn channels (3-29) are available to the user application.

This is captured in the System Interrupt PDL documentation. TRM captures the device capabilities and since these usage is a software/firmware wrapper to implement certain system level functions, these details are not captured in TRM.

Let me know if this helps.

Regards,

Meenakshi Sundaram R

View solution in original post

3 Replies
MeenakshiR_71
Employee
Employee
100 likes received 50 likes received 25 likes received

Hello,

Yes M0+ allows 32 interrupts as captured in TRM. However, CM0+ interrupt channels 0-2 and 30-31 are reserved for system use, inter-processor communication, and the crypto driver. Other IRQn channels (3-29) are available to the user application.

This is captured in the System Interrupt PDL documentation. TRM captures the device capabilities and since these usage is a software/firmware wrapper to implement certain system level functions, these details are not captured in TRM.

Let me know if this helps.

Regards,

Meenakshi Sundaram R

Anonymous
Not applicable

Hello,

Thanks.

I find the sentence in Cypress Peripheral Driver Library 3.0.1 (build 716). TRM you said is for PDL?

If yes, I can not find the TRM.

Is that TRM opend?

Best regards,

0 Likes

TRM does not include the information because TRM only captures device capabilities in hardware. The implementation is a software wrapper and hence captured only in PDL documentation.

Regards,

Meenakshi Sundaram R

0 Likes