Signal generator_PSOC 6

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
aliissa02
Level 4
Level 4
100 sign-ins 50 replies posted 5 likes given

Hello,

I am trying to generate a frequency of 6 MHz using a Psoc 6 prototyping bord. Can you please check the attached project if this is correct?

Thank you

0 Likes
1 Solution
Arpit_S
Moderator
Moderator
Moderator
250 replies posted 100 solutions authored 250 sign-ins

Hi,

Yes, In the project attached, The PWM component is getting a clock source of 6MHz and the effective counting frequency is 6250KHz. Also, for further information: In case you want to use some other frequency value make sure to use Clock Prescalar in the PWM Configurator. For more details refer to https://www.infineon.com/dgdl/Infineon-PSoC_6_MCU_PSoC_62_Architecture_Technical_Reference_Manual-Ad... Section 20.7 Peripheral Clock Divider

Kind Regards

Arpit Srivastav

View solution in original post

0 Likes
1 Reply
Arpit_S
Moderator
Moderator
Moderator
250 replies posted 100 solutions authored 250 sign-ins

Hi,

Yes, In the project attached, The PWM component is getting a clock source of 6MHz and the effective counting frequency is 6250KHz. Also, for further information: In case you want to use some other frequency value make sure to use Clock Prescalar in the PWM Configurator. For more details refer to https://www.infineon.com/dgdl/Infineon-PSoC_6_MCU_PSoC_62_Architecture_Technical_Reference_Manual-Ad... Section 20.7 Peripheral Clock Divider

Kind Regards

Arpit Srivastav

0 Likes