cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 6

Pritam
New Contributor

When I  run the program in MODUS toolbox I get this type of error.What to do? AND some time I am also getting BAUDRATE error

/////////////////////////////////////////////////////////

Programming target device ...

Found serial port : COM4

Downloading FW ...
Failed to execute DownloadMinidriver command
Download failed

If the serial port was not detected, make sure no other program such as ClientControl has the port open.

If you have issues downloading to the kit, follow the steps below:

Press and hold the 'Recover' button on the kit.
Press and hold the 'Reset' button on the kit.
Release the 'Reset' button.
After one second, release the 'Recover' button.
make[1]: *** [../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v3.1.0/COMPONENT_20706A2/make/recipe/program.mk:102: qprogram] Error 1
make: *** [../mtb_shared/core-make/release-v1.8.0/make/core/main.mk:426: secondstage_build] Error 2

0 Likes
1 Solution
DheerajPK_41
Moderator
Moderator

Hi,

Have you recovered the device properly as in the error message? 

Also, could you please try connect the HCI UART CTS pin to ground using fly-wires and try programming again?

 

Thanks,

-Dheeraj.P.K

View solution in original post

0 Likes
2 Replies
DheerajPK_41
Moderator
Moderator

Hi,

Have you recovered the device properly as in the error message? 

Also, could you please try connect the HCI UART CTS pin to ground using fly-wires and try programming again?

 

Thanks,

-Dheeraj.P.K

View solution in original post

0 Likes
Top labels