- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am facing some trouble with ADC running in continuous mode. It is really simple code which I write using modus toolbox. I did some setting in modux toolbox device configurator for CY8C6244LQI-S4D92 device. I am using CY8CKIT-062S4 PSoC 62S4 pioneer board.
The code generated from the configuration is :
--------------------------
/* NOTE: This is a preview only. It combines elements of the
* cycfg_peripherals.c and cycfg_peripherals.h files located in the folder
* C:/Users/agarwaln/mtw2/Asymmetric_PWM_Generation/COMPONENT_CUSTOM_DESIGN_MODUS/TARGET_CY8CKIT-062S4/GeneratedSource.
*/
#include "cy_sar.h"
#include "cycfg_routing.h"
#include "cy_sysclk.h"
#if defined (CY_USING_HAL)
#include "cyhal_hwmgr.h"
#endif //defined (CY_USING_HAL)
#define pass_0_saradc_0_sar_0_HW SAR0
#define pass_0_saradc_0_sar_0_IRQ pass_interrupt_sar_IRQn
#define pass_0_saradc_0_sar_0_CTL ((uint32_t)CY_SAR_VREF_PWR_100 | (uint32_t)CY_SAR_VREF_SEL_VDDA | (uint32_t)CY_SAR_BYPASS_CAP_DISABLE | (uint32_t)CY_SAR_NEG_SEL_VSSA_KELVIN | (uint32_t)CY_SAR_CTRL_NEGVREF_HW | (uint32_t)CY_SAR_CTRL_COMP_DLY_12 | (uint32_t)CY_SAR_COMP_PWR_100 | (uint32_t)CY_SAR_DEEPSLEEP_SARMUX_OFF | (uint32_t)CY_SAR_SARSEQ_SWITCH_ENABLE)
#define pass_0_saradc_0_sar_0_SAMPLE ((uint32_t)SAR_SAMPLE_CTRL_EOS_DSI_OUT_EN_Msk | (uint32_t)CY_SAR_RIGHT_ALIGN | (uint32_t)CY_SAR_DIFFERENTIAL_SIGNED | (uint32_t)CY_SAR_SINGLE_ENDED_SIGNED | (uint32_t)CY_SAR_AVG_CNT_2 | (uint32_t)CY_SAR_AVG_MODE_SEQUENTIAL_FIXED | (uint32_t)CY_SAR_TRIGGER_MODE_FW_ONLY)
#define pass_0_saradc_0_sar_0_CH0_CONFIG (((uint32_t)SAR0_VPLUS0_PORT << SAR_CHAN_CONFIG_POS_PORT_ADDR_Pos) | (uint32_t)(SAR0_VPLUS0_PIN << SAR_CHAN_CONFIG_POS_PIN_ADDR_Pos) | CY_SAR_CHAN_SINGLE_ENDED | CY_SAR_CHAN_AVG_DISABLE | (uint32_t)CY_SAR_CHAN_SAMPLE_TIME_0)
#define pass_0_saradc_0_sar_0_VREF_MV 3300UL
const cy_stc_sar_config_t pass_0_saradc_0_sar_0_config =
{
.ctrl = (uint32_t) pass_0_saradc_0_sar_0_CTL,
.sampleCtrl = (uint32_t) pass_0_saradc_0_sar_0_SAMPLE,
.sampleTime01 = (76UL << (uint32_t)CY_SAR_SAMPLE_TIME0_SHIFT) | (2UL << (uint32_t)CY_SAR_SAMPLE_TIME1_SHIFT),
.sampleTime23 = (2UL << (uint32_t)CY_SAR_SAMPLE_TIME2_SHIFT) | (2UL << (uint32_t)CY_SAR_SAMPLE_TIME3_SHIFT),
.rangeThres = (0UL << (uint32_t)CY_SAR_RANGE_HIGH_SHIFT) | (0UL << (uint32_t)CY_SAR_RANGE_LOW_SHIFT),
.rangeCond = CY_SAR_RANGE_COND_BELOW,
.chanEn = 1UL,
.chanConfig = {(uint32_t) pass_0_saradc_0_sar_0_CH0_CONFIG, 0UL, 0UL, 0UL, 0UL, 0UL, 0UL, 0UL, 0UL, 0UL, 0UL, 0UL, 0UL, 0UL, 0UL, 0UL, 0UL},
.intrMask = CY_SAR_INTR_EOS,
.satIntrMask = 0UL,
.rangeIntrMask = 0UL,
.configRouting = false,
.vrefMvValue = pass_0_saradc_0_sar_0_VREF_MV,
.clock = CY_SAR_CLK_PERI,
.fifoCfgPtr = NULL,
.trTimer = false,
.scanCnt = false,
.scanCntIntr = true,
};
#if defined (CY_USING_HAL)
const cyhal_resource_inst_t pass_0_saradc_0_sar_0_obj =
{
.type = CYHAL_RSC_ADC,
.block_num = 0,
.channel_num = 0,
};
#endif //defined (CY_USING_HAL)
void init_cycfg_peripherals(void)
{
SAR_MUX_SWITCH0(pass_0_saradc_0_sar_0_HW) |= CY_SAR_MUX_FW_VSSA_VMINUS;
SAR_MUX_SWITCH_SQ_CTRL(pass_0_saradc_0_sar_0_HW) |= CY_SAR_MUX_SQ_CTRL_VSSA;
Cy_SysClk_PeriphAssignDivider(PCLK_PASS_CLOCK_SAR0, CY_SYSCLK_DIV_8_BIT, 2U);
#if defined (CY_USING_HAL)
cyhal_hwmgr_reserve(&pass_0_saradc_0_sar_0_obj);
#endif //defined (CY_USING_HAL)
}
------------------------
In the main.c file the code is:
-------------------
int main(void)
{
cy_rslt_t result;
cy_en_sar_status_t status;
/* Initialize the device and board peripherals */
result = cybsp_init() ;
if (result != CY_RSLT_SUCCESS)
{
CY_ASSERT(0);
}
#ifdef PORT_TOGGLE
/* Port and pin translations for the USER_LED */
CYBSP_USER_LED_PORT = CYHAL_GET_PORTADDR(CYBSP_USER_LED);
CYBSP_USER_LED_PIN = CYHAL_GET_PIN(CYBSP_USER_LED);
/* Initialize USER_LED */
Cy_GPIO_Pin_FastInit(CYBSP_USER_LED_PORT, CYBSP_USER_LED_PIN, CY_GPIO_DM_STRONG, 0UL, HSIOM_SEL_GPIO);
#endif
status = Cy_SAR_Init(pass_0_saradc_0_sar_0_HW, &pass_0_saradc_0_sar_0_config);
if (CY_SAR_SUCCESS == status)
{
/* Turn on the SAR hardware. */
Cy_SAR_Enable(pass_0_saradc_0_sar_0_HW);
/* Begin continuous conversions. */
Cy_SAR_StartConvert(pass_0_saradc_0_sar_0_HW, 1);
}
/* Variable to store ADC conversion result from channel 0 */
int32_t adc_result_0 = 0;
for(;;)
{
/* 200ms delay between scans */
cyhal_system_delay_ms(200);
/* Read input voltage, convert it to millivolts and print input voltage */
adc_result_0 = Cy_SAR_GetResult32(pass_0_saradc_0_sar_0_HW,0);
}
-------------------
I am checking value of SAR0 registers after running the code for a while. Please find attached the different registers values. I have connected the the pin10_0 to V3.3. The result resister is always shows 0xF800 while I am expecting 0x07FF. It never changes even if I connect the P10_0 to GND.
When I run the example code, the ADC result value is showing expected result. Is there any initialization missing in the code or configuration?
Could you please check the issue?
Solved! Go to Solution.
- Labels:
-
PSoC 6 MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Can you call Cy_SAR_IsEndConversion with CY_SAR_WAIT_FOR_RESULT as the parameter before reading the result ?
Best Regard,
Vasanth
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Can you call Cy_SAR_IsEndConversion with CY_SAR_WAIT_FOR_RESULT as the parameter before reading the result ?
Best Regard,
Vasanth
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks Vasanth for your response!
The problem is solved now.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Yes, The problem is solved now.
Thankyou,