Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 6 Forum Discussions

DaGa_4352226
Level 2
Level 2
10 questions asked 5 replies posted 5 questions asked

Hello Community

I'm using a Kit CY8CKIT-062-BLE and I want to write some data into the chip and later read it again. After the server/BLE is turn off, it should be not erease.

I know this chip has 4 block of 512 bytes each. but how I can get access to the address and how long it should be?

The value ,that i want to save and to read, is a uint8_t format.

Which method should I use to save the value and read it later?

Thanks, regards

David

0 Likes
1 Solution
Yugandhar
Moderator
Moderator
Moderator
1000 replies posted 5 likes given First comment on blog

Hello David,

Yes, in PSoC6 BLE there is a user row in SFLASH which is used for storing the user data. But, I would recommend you to use the Emulated EEPROM area (32 KB of flash) for storing. Please refer to the code example "CE195313_PSoC_EmEEPROM_PSoC6" in the PSoC Creator or from CE195313 for more information on using the Em_EEPROM component.

Thanks,

P Yugandhar.

View solution in original post

0 Likes
1 Reply
Yugandhar
Moderator
Moderator
Moderator
1000 replies posted 5 likes given First comment on blog

Hello David,

Yes, in PSoC6 BLE there is a user row in SFLASH which is used for storing the user data. But, I would recommend you to use the Emulated EEPROM area (32 KB of flash) for storing. Please refer to the code example "CE195313_PSoC_EmEEPROM_PSoC6" in the PSoC Creator or from CE195313 for more information on using the Em_EEPROM component.

Thanks,

P Yugandhar.

0 Likes