Questions about ECO for CYBLE-416045-02

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
TaTa_2447651
Level 3
Level 3
First solution authored 25 replies posted 10 replies posted

Looking at the data sheet of CYBLE-416045-02, there is a block diagram written as ECO for BLE as below.

Does this mean that ECO is installed inside CYBLE-416045-02?

Or do I need to prepare an ECO and input it to the microcomputer?

Best regards.

--------

CYBLE-416045-02のデータシートを見ると以下のようにECO for BLEと書かれているブロック図があります。

これはCYBLE-416045-02の内部にECOが搭載されているということでしょうか?

それとも自分でECOを用意してマイコンに入力する必要があるということでしょうか?

--------

pastedImage_0.png

0 Likes
1 Solution
ShipingW_81
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Yes, there is already a BLE ECO mounted inside CYBLE-416045-02 module. You can use BLE ECO as clock source of main system through enabling AltHF clock. That means there is no need to add ECO outside the module.

View solution in original post

2 Replies
ShipingW_81
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Yes, there is already a BLE ECO mounted inside CYBLE-416045-02 module. You can use BLE ECO as clock source of main system through enabling AltHF clock. That means there is no need to add ECO outside the module.

Hi, WangS_81.

Thank you for your answer.

0 Likes